charging battery

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

charging battery

2,257件の閲覧回数
idom
Contributor II

Hi

I use IMX8MMEVKHUG as a reference design.

Does the USB-OTG design support battery charging?

Is there any UG can guide me to connect 5.5-8V LI-PO to the design?

if I connect a battery to J101 will charge it  ?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,133件の閲覧回数
idom
Contributor II

I am looking for full datasheet of NX20P3483UK and PCA9468

Do you have any application note for PCA9468

0 件の賞賛
返信

2,133件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Ido,

We don´t have a User Guide for the USB, but we have the general user guide you can downloaded from:

https://www.nxp.com/webapp/Download?colCode=IMX8MMEVKHUG 

https://www.nxp.com/webapp/Download?colCode=IMX8MMHDG 

On the board side There are two USB:

J301 is connected to the USB1 interface of the i.MX 8M Mini, which can act as the download port of the EVK.
J302 is connected to the USB2 interface of the i.MX 8M Mini, which can act as the power supply port of the EVK.

Regards

0 件の賞賛
返信