changes to be made in u-boot for changing from DDR3 to LPDDR2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

changes to be made in u-boot for changing from DDR3 to LPDDR2

1,051 Views
srinivasaporam
Contributor II

Hi,

We have  got a customized board which is designed based on Freescale's IMX6Q/IMX6DL processor board. This customized board is using LPDDR2  where as reference board is having DDR3 memory. And also reference board is designed with IMX6Q/IMX6DL where as customized board is based on IMX6D.

Now, what are the changes that we need to do in U-boot. Which are all the files those need to be modified.

Labels (4)
Tags (1)
0 Kudos
Reply
2 Replies

912 Views
igorpadykov
NXP Employee
NXP Employee

Hi Srinivasa

changes are *.cfg file with ddr configuration, location

../uboot/board/freescale/mx6sabresd and ..include/configs/*.h

board file.

Best regards

igor

0 Kudos
Reply

912 Views
srinivasaporam
Contributor II

Hi,

But my board is based on reference designs of wandboard.

0 Kudos
Reply