cannot multiplex flexcan1 on LCD pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

cannot multiplex flexcan1 on LCD pins

3,076 Views
netfish
Contributor I

Hello,

We are using i.mx6ul mpu and multiplexing flexcan1 on pins LCD_DATA08 & LCD_DATA09, but no luck.

dts changed as follows:

pinctrl_flexcan1: flexcan1grp{
    fsl,pins = <
        MX6UL_PAD_LCD_DATA08__FLEXCAN1_TX 0x1b020
        MX6UL_PAD_LCD_DATA09__FLEXCAN1_RX 0x1b020
    >;
};

No signal occurs on the LCD_DATA08 pin when can sending, checked using oscilloscope.

What issue can it be? Any special care should be taken when using LCD pins?

We are stuck on this for nearly a week.  Any response is appreciated.

Thanks,

Edwin

0 Kudos
Reply
5 Replies

2,900 Views
igorpadykov
NXP Employee
NXP Employee

Hi Edwin

i.MX6UL flexcan1 example can be found on

linux/arch/arm/boot/dts/imx6ul-14x14-evk.dts

imx6ul-14x14-evk.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

One can check if these lcd MX6UL_PAD_LCD_DATA08 pads were not used

by other modules. Also recommended to testing attach another board, otherwise

you may will not see flexcan signals.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,900 Views
netfish
Contributor I

Hi igor,

 

Thanks for your reply.

We have double checked. No othrer moudle use these pins. 

We have tried to route flexcan1_tx to other pins, it is OK.

Our board is mostly compatible with NXP official IMX6UL-EVK.

LCD_DATA08 is attached directly to can receiver with a 10k pull-down resistor for boot.

pastedImage_5.png

Are there any special power or clock settings needed?

pinctrl_flexcan1: flexcan1grp{
fsl,pins = <
//MX6UL_PAD_UART3_RTS_B__FLEXCAN1_RX 0x1b020
//MX6UL_PAD_UART3_CTS_B__FLEXCAN1_TX 0x1b020
MX6UL_PAD_LCD_DATA08__FLEXCAN1_TX 0x1b020
MX6UL_PAD_LCD_DATA09__FLEXCAN1_RX 0x1b020
//MX6UL_PAD_SD1_DATA0__FLEXCAN1_TX 0x1b020
//MX6UL_PAD_SD1_DATA1__FLEXCAN1_RX 0x1b020
>;
};

pinctrl_lcdif_dat: lcdifdatgrp {
fsl,pins = <
MX6UL_PAD_LCD_DATA00__LCDIF_DATA00 0x79
MX6UL_PAD_LCD_DATA01__LCDIF_DATA01 0x79
MX6UL_PAD_LCD_DATA02__LCDIF_DATA02 0x79
MX6UL_PAD_LCD_DATA03__LCDIF_DATA03 0x79
MX6UL_PAD_LCD_DATA04__LCDIF_DATA04 0x79
MX6UL_PAD_LCD_DATA05__LCDIF_DATA05 0x79
MX6UL_PAD_LCD_DATA06__LCDIF_DATA06 0x79
MX6UL_PAD_LCD_DATA07__LCDIF_DATA07 0x79
//MX6UL_PAD_LCD_DATA08__LCDIF_DATA08 0x79
//MX6UL_PAD_LCD_DATA09__LCDIF_DATA09 0x79
MX6UL_PAD_LCD_DATA10__LCDIF_DATA10 0x79
MX6UL_PAD_LCD_DATA11__LCDIF_DATA11 0x79
MX6UL_PAD_LCD_DATA12__LCDIF_DATA12 0x79
MX6UL_PAD_LCD_DATA13__LCDIF_DATA13 0x79
MX6UL_PAD_LCD_DATA14__LCDIF_DATA14 0x79
MX6UL_PAD_LCD_DATA15__LCDIF_DATA15 0x79
MX6UL_PAD_LCD_DATA16__LCDIF_DATA16 0x79
MX6UL_PAD_LCD_DATA17__LCDIF_DATA17 0x79
MX6UL_PAD_LCD_DATA18__LCDIF_DATA18 0x79
MX6UL_PAD_LCD_DATA19__LCDIF_DATA19 0x79
MX6UL_PAD_LCD_DATA20__LCDIF_DATA20 0x79
MX6UL_PAD_LCD_DATA21__LCDIF_DATA21 0x79
MX6UL_PAD_LCD_DATA22__LCDIF_DATA22 0x79
MX6UL_PAD_LCD_DATA23__LCDIF_DATA23 0x79
>;
};

Any advice?

Thanks,

Edwin

0 Kudos
Reply

2,900 Views
zzyhqu
Contributor I

Hi Edwin ,

did you resolve your problem and how to resolve it ? I also meet the same problem

0 Kudos
Reply

2,900 Views
netfish
Contributor I

Hi xm,

No. We just rebuilt our board and route the can to uart3 rts/cts.

0 Kudos
Reply

2,900 Views
igorpadykov
NXP Employee
NXP Employee

Hi Edwin

lcd can be used in uboot splashscreen, so one can try to disable these pins

in uboot too, please check iomux_v3_cfg_t const lcd_pads[]:
mx6ul_14x14_evk.c\mx6ul_14x14_evk\freescale\board - uboot-imx - i.MX U-Boot 

Also as signal LCDIF_DATA08 has not alternative mux option except from pad

MX6UL_PAD_LCD_DATA08__LCDIF_DATA08, seems one can disable lcd completely.

Best regards
igor

0 Kudos
Reply