can we port android on linux on I.MX6 board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

can we port android on linux on I.MX6 board

865件の閲覧回数
shalinikp
Contributor II

can we port android on linux on I.MX6 board ?

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

756件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Sorry, we do not have special notes about Android porting.

Nevertheless, hope the following helps.

Port Android to custom board


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

756件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi shalini

please check below ready Freescale Android releases (they are based on Linux),

may be they will suit.

Operating System Software-Board Support Packages (33)

i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale

Best regards

igor

0 件の賞賛
返信