hi,
i am using imx6sl custom boad and android4.4, i find a problem and don't know how to deal it .
can anyone give me some s guid?
filesystem can not mount sucessful! look the log, emmc write timeout ! why? thanks everyone!
U-Boot 2009.08-dirty ( 4鏈26 2016 - 10:17:15)
U-Boot code: 87800640 -> 87833000 BSS: -> 8786DC30
CPU: Freescale i.MX6 family TO1.2 at 396 MHz
Thermal sensor with ratio = 185
Temperature: 41 C, calibration data 0x5945175f
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock : 49500000Hz
ipg per clock : 49500000Hz
uart clock : 80000000Hz
cspi clock : 60000000Hz
ahb clock : 99000000Hz
axi clock : 198000000Hz
emi_slow clock: 99000000Hz
ddr clock : 396000000Hz
usdhc1 clock : 198000000Hz
usdhc2 clock : 198000000Hz
usdhc3 clock : 198000000Hz
usdhc4 clock : 198000000Hz
Board: MX6SoloLite-EVK (0x60312): [ POR ]
Boot Device: MMC
I2C: ready
RAM Configuration:
Bank #0: 80000000 1.2 GB
MMC: FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2
In: serial
Out: serial
Err: serial
Found PFUZE100! deviceid=10,revid=21
Net: got MAC address from IIM: 00:00:00:00:00:00
FEC0 [PRIME]
### main_loop entered: bootdelay=3
### main_loop: bootcmd="booti mmc0"
Hit any key to stop autoboot: 0
lining debug abortboot return abort = 0
ptn 0 name='boot' start=53248 len=27262976
booti: mmc read kernel pte->start = 0x0000d000
booti: mmc read kernel hdr->page_size = 2048
booti: mmc read kernel mmcc = 0
booti: mmc read kernel sector = 0x0000d004
booti: mmc read kernel (hdr->kernel_size / 512) + 1 = 9324
booti: mmc read kernel (void *)hdr->kernel_addr = 0x80800000
Image magic: ANDROID!
譎
kernel_size: 0x48d70c
kernel_addr: 0x80800000
rdisk_size: 0x79b0d
rdisk_addr: 0x81800000
second_size: 0x0
second_addr: 0x81700000
tags_addr: 0x80800100
page_size: 0x800
name:
cmdline: console=ttymxc0,115200 init=/init tps65185:pass=2,vcom=-2030000 video=mxcepdcfb:E97_V110,bpp=16 androidboot.console=ttymxc0 video=mxc_elcdif_fb:off androidboot.hardware=freescale2020000
id[0]: 0x0
id[1]: 0x0
id[2]: 0x0
id[3]: 0x0
id[4]: 0x0
id[5]: 0x0
id[6]: 0x0
id[7]: 0x0
kernel @ 80800000 (4773644)
ramdisk @ 81800000 (498445)
kernel cmdline:
use boot.img command line:
console=ttymxc0,115200 init=/init tps65185:pass=2,vcom=-2030000 video=mxcepdcfb:E97_V110,bpp=16 androidboot.console=ttymxc0 video=mxc_elcdif_fb:off androidboot.hardware=freescale androidboot.serialno=0b27b1d4df669563
params->u.mem.start = 0x80000000
params->u.mem.size = 0x7fffffff
Starting kernel ...
Initializing cgroup subsys cpuset
Initializing cgroup subsys cpu
Linux version 3.0.35-06532-gdfe90de-dirty (root@HP-Z230-Workstation) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #151 PREEMPT Thu Jun 23 18:02:09 CST 2016
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Freescale i.MX 6SoloLite EVK Board
Memory policy: ECC disabled, Data cache writeback
CPU identified as i.MX6SoloLite, silicon rev 1.2
On node 0 totalpages: 511999
free_area_init_node: node 0, pgdat c0cb0d04, node_mem_map c187a000
Normal zone: 1344 pages used for memmap
Normal zone: 0 pages reserved
Normal zone: 170688 pages, LIFO batch:31
HighMem zone: 2752 pages used for memmap
HighMem zone: 337215 pages, LIFO batch:31
pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
pcpu-alloc: [0] 0
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 507903
Kernel command line: console=ttymxc0,115200 init=/init tps65185:pass=2,vcom=-2030000 video=mxcepdcfb:E97_V110,bpp=16 androidboot.console=ttymxc0 video=mxc_elcdif_fb:off androidboot.hardware=freescale androidboot.serialno=0b27b1d4df669563
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 1999MB = 1999MB total
Memory: 2016064k/2016064k available, 81084k reserved, 1359868K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xfbe00000 - 0xffe00000 ( 64 MB)
vmalloc : 0xea800000 - 0xf2000000 ( 120 MB)
lowmem : 0xc0000000 - 0xea000000 ( 672 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.init : 0xc0008000 - 0xc0038000 ( 192 kB)
.text : 0xc0038000 - 0xc0c4c668 (12370 kB)
.data : 0xc0c4e000 - 0xc0cb18c0 ( 399 kB)
.bss : 0xc0cb18e4 - 0xc0ddea48 (1205 kB)
Preemptible hierarchical RCU implementation.
NR_IRQS:624
MXC GPIO hardware
sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956ms
*************reg:0xc0011740*********
arm_max_freq=1GHz
MXC_Early serial console at MMIO 0x2020000 (options '115200')
bootconsole [ttymxc0] enabled
Calibrating delay loop... 789.70 BogoMIPS (lpj=3948544)
pid_max: default: 32768 minimum: 301
Security Framework initialized
Mount-cache hash table entries: 512
vfs_kern_mount 1
vfs_kern_mount 2
vfs_kern_mount 3
mount_fs 1
mount_fs 3
mount_fs 4
mount_fs 5
mount_fs 6
mount_fs 7
mount_fs 8
vfs_kern_mount 5
do_kern_mount1
vfs_kern_mount 1
vfs_kern_mount 2
vfs_kern_mount 3
mount_fs 1
mount_fs 3
mount_fs 4
mount_fs 5
mount_fs 6
mount_fs 7
mount_fs 8
vfs_kern_mount 5
do_kern_mount3
vfs_kern_mount 1
vfs_kern_mount 2
vfs_kern_mount 3
mount_fs 1
mount_fs 3
mount_fs 4
mount_fs 5
mount_fs 6
mount_fs 7
mount_fs 8
vfs_kern_mount 5
vfs_kern_mount 1
vfs_kern_mount 2
vfs_kern_mount 3
mount_fs 1
mount_fs 2
mount_fs 3
mount_fs 4
mount_fs 5
mount_fs 6
mount_fs 7
mount_fs 8
vfs_kern_mount 5
CPU: Testing write buffer coherency: ok
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
vfs_kern_mount 1
vfs_kern_mount 2
vfs_kern_mount 3
mount_fs 1
mount_fs 3
mount_fs 4
mount_fs 5
mount_fs 6
mount_fs 7
mount_fs 8
vfs_kern_mount 5
vfs_kern_mount 1
vfs_kern_mount 2
vfs_kern_mount 3
mount_fs 1
mount_fs 3
mount_fs 4
mount_fs 5
mount_fs 6
mount_fs 7
mount_fs 8
vfs_kern_mount 5
vfs_kern_mount 1
vfs_kern_mount 2
vfs_kern_mount 3
mount_fs 1
mount_fs 3
mount_fs 4
mount_fs 5
mount_fs 6
mount_fs 7
mount_fs 8
vfs_kern_mount 5
NET: Registered protocol family 16
->drivers/i2c/i2c-boardinfo.c:i2c_register_board_info :0
->bus_num 0:0 rt9428:0x36
->bus_num 0:1 tps65185:0x68
->drivers/i2c/i2c-boardinfo.c:i2c_register_board_info :1
->drivers/i2c/i2c-boardinfo.c:i2c_register_board_info :2
->drivers/i2c/i2c-boardinfo.c:i2c_register_board_info :3
->bus_num 0:0 pfuze100:0x8
hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.
hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.
hw-breakpoint: maximum watchpoint size is 4 bytes.
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x32030000, Cache size: 262144 B
bio: create slab <bio-0> at 0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
Freescale USB OTG Driver loaded, $Revision: 1.55 $
mc_pfuze 0-0008: ID: 0,Full lay: 2 ,Metal lay: 1
mc_pfuze 0-0008: FAB: 0 ,FIN: 0
->pfuze100_init
->pfuze100 version:21
->pfuze100 VGEN1 CTL:18
->pfuze100 VGEN1 VOLT:0
->pfuze100 VGEN1 VOLT:0
->pfuze100 VGEN1 CTL:18
->pfuze100 init end
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Version 1.0.24.
NET: Registered protocol family 23
Bluetooth: Core ver 2.16
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
cfg80211: Calling CRDA to update world regulatory domain
-----------tps65185_probe---------
client->name = tps65185, client->addr = 0x68
i2c-core: driver [tps65185] using legacy suspend method
i2c-core: driver [tps65185] using legacy resume method
rt_fg_get_property: FG_SOC=1020, SYS_SOC=100
rt_fg_get_property: FG_SOC=1020, SYS_SOC=100
add wake up source irq 105
rt9428 0-0036: driver successfully loaded
i2c-core: driver [rt9428] using legacy suspend method
i2c-core: driver [rt9428] using legacy resume method
Switching to clocksource mxc_timer1
vfs_kern_mount 1
vfs_kern_mount 2
vfs_kern_mount 3
mount_fs 1
mount_fs 3
mount_fs 4
mount_fs 5
mount_fs 6
mount_fs 7
mount_fs 8
vfs_kern_mount 5
vfs_kern_mount 1
vfs_kern_mount 2
vfs_kern_mount 3
mount_fs 1
mount_fs 3
mount_fs 4
mount_fs 5
mount_fs 6
mount_fs 7
mount_fs 8
vfs_kern_mount 5
FS-Cache: Loaded
CacheFiles: Loaded
NET: Registered protocol family 2
IP route cache hash table entries: 32768 (order: 5, 131072 bytes)
TCP established hash table entries: 131072 (order: 8, 1048576 bytes)
TCP bind hash table entries: 65536 (order: 6, 262144 bytes)
TCP: Hash tables configured (established 131072 bind 65536)
TCP reno registered
UDP hash table entries: 512 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 512 (order: 1, 8192 bytes)
/**************rt9428_dwork_func************/
/**************rt9428_update_info************/
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Unpacking initramfs...
rt9428_update_info: REG_CFG = 0x325f
rt9428_update_info: REG_STATUS = 0x0000
rt9428_update_info: FG_VBAT = 4295
rt9428_update_info: ORG_TEMP = 31, TEMP = 25
rt9428_update_info: FG_SOC = 1020
rt9428_update_info: VG1 = 0x8132
Freeing initrd memory: 484K
etb: probe of etb failed with error -2
etm: probe of etm.0 failed with error -2
rt9428_update_info: VG2 = 0x8232
Static Power Management for Freescale i.MX6
wait mode is enabled for i.MX6
cpaddr = ea820000 suspend_iram_base=ea818000
PM driver module loaded
IMX usb wakeup probe
rt9428_update_info: VG3 = 0x8332
the wakeup pdata is 0xe616df60
add wake up source irq 75
rt9428_update_info: VG4 = 0x8332
IMX usb wakeup probe
the wakeup pdata is 0xe616dd60
rt9428_update_info: CVS = 0x8332
/**************rt9428_update_info**end**********/
cpu regulator mode:ldo_bypass
rt_fg_get_property: FG_SOC=1020, SYS_SOC=100
_regulator_get: get() with no identifier
mx6_cpu_regulator_init: failed to get pu regulator
i.MXC CPU frequency driver
audit: initializing netlink socket (disabled)
type=2000 audit(0.800:1): initialized
highmem bounce pool size: 64 pages
ashmem: initialized
vfs_kern_mount 1
vfs_kern_mount 2
vfs_kern_mount 3
mount_fs 1
mount_fs 3
mount_fs 4
mount_fs 5
mount_fs 6
mount_fs 7
mount_fs 8
vfs_kern_mount 5
vfs_kern_mount 1
vfs_kern_mount 2
vfs_kern_mount 3
mount_fs 1
mount_fs 3
mount_fs 4
mount_fs 5
mount_fs 6
mount_fs 7
mount_fs 8
vfs_kern_mount 5
NTFS driver 2.1.30 [Flags: R/O].
JFFS2 version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.
fuse init (API version 7.16)
msgmni has been set to 1282
NET: Registered protocol family 38
cryptodev: driver loaded.
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-sdma imx-sdma: loaded firmware 1.1
imx-sdma imx-sdma: initialized
Serial: IMX driver
imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX
console [ttymxc0] enabled, bootconsole disabled
console [ttymxc0] enabled, bootconsole disabled
loop: module loaded
vfs_kern_mount 1
vfs_kern_mount 2
vfs_kern_mount 3
mount_fs 1
mount_fs 3
mount_fs 4
mount_fs 5
mount_fs 6
mount_fs 7
mount_fs 8
vfs_kern_mount 5
PPP generic driver version 2.4.2
PPP Deflate Compression module registered
PPP BSD Compression module registered
PPP MPPE Compression module registered
NET: Registered protocol family 24
RTL871X: module init start
RTL871X: rtl8189es v4.3.10_12447.20141008
RTL871X: build time: Jun 12 2016 10:31:48
RTL871X: module init ret=0
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1
fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000
fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00
usb usb1: usb_autoresume_device: cnt 5 -> 1
usb usb1: usb_autoresume_device: cnt 6 -> 1
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
usb usb1: usb_autosuspend_device: cnt 4 -> 0
usb usb1: usb_autosuspend_device: cnt 3 -> 0
add wake up source irq 74
fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2
fsl-ehci fsl-ehci.1: irq 74, io base 0x02184200
fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00
usb usb2: usb_autoresume_device: cnt 5 -> 1
usb usb2: usb_autoresume_device: cnt 6 -> 1
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
usb usb2: usb_autosuspend_device: cnt 4 -> 0
usb usb2: usb_autosuspend_device: cnt 3 -> 0
usbcore: registered new interface driver cdc_acm
hub 1-0:1.0: usb_autopm_put_interface_async: cnt 1 -> 0
hub 1-0:1.0: usb_autopm_get_interface: cnt 2 -> 1
cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
Initializing USB Mass Storage driver...
hub 1-0:1.0: usb_autopm_put_interface: cnt 0 -> 0
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
usbcore: registered new interface driver usbserial
usbserial: USB Serial Driver core
USB Serial support registered for GSM modem (1-port)
usbcore: registered new interface driver option
option: v0.7.2:USB Driver for GSM modems
USB Serial support registered for Qualcomm USB modem
usbcore: registered new interface driver qcserial
ARC USBOTG Device Controller driver (1 August 2005)
imx6 usb charger online:0
android_usb gadget: Mass Storage Function, version: 2009/09/11
hub 2-0:1.0: usb_autopm_put_interface_async: cnt 1 -> 0
hub 2-0:1.0: usb_autopm_get_interface: cnt 2 -> 1
hub 2-0:1.0: usb_autopm_put_interface: cnt 0 -> 0
android_usb gadget: Number of LUNs=1
lun0: LUN: removable file: (no medium)
Gadget Android: controller 'fsl-usb2-udc' not recognized
android_usb gadget: android_usb ready
Suspend udc for OTG auto detect
USB Host suspend begins
will suspend roothub and its children
hub 1-0:1.0: usb_suspend_interface: status 0
ehci_fsl_bus_suspend begins, DR
ehci_fsl_bus_suspend ends, DR
usb usb1: usb_suspend_device: status 0
usb usb1: usb_suspend_both: status 0
host suspend ends
USB Gadget resume begins
fsl_udc_resume, Wait for wakeup thread finishes
dr_controller_run: udc out low power mode
USB Gadget resume ends
fsl-usb2-udc: bind to driver android_usb
input: imx-keypad as /devices/platform/imx-keypad/input/input0
-----code:102 val:0-----
-----code:114 val:0-----
-----code:115 val:0-----
-----code:105 val:0-----
-----code:106 val:0-----
add wake up source irq 103
----------pen probe-------------------
---uart clk is:80000000-----------
-----pen_tablet_init--------
-----pen_tablet_power----status = 0--
---------uart2 gpio init---------
-----pen_tablet_power----status = 1--
---------uart2 init---------
imx-uart.1: ttymxc1 at MMIO 0x2024000 (irq = 59) is a IMX
--------serial_8250_probe:612---------
--------serial_8250_startup:324---------
UCR1:0
UCR2:1
UCR3:700
UCR4:8000
UFCR:801
USR1:2040
USR2:4008
UBIR:0
UBMR:0
UBRC:4
UTS:60
--------serial_8250_startup:341---------
UCR1:1
UCR2:1
UCR3:700
UCR4:8000
UFCR:801
USR1:2040
USR2:4008
UBIR:0
UBMR:0
UBRC:4
UTS:60
--------serial_8250_startup:345---------
UCR1:1
UCR2:6027
UCR3:700
UCR4:8000
UFCR:801
USR1:2040
USR2:5008
UBIR:0
UBMR:0
UBRC:4
UTS:60
--------serial_8250_startup:349---------
UCR1:1
UCR2:6027
UCR3:700
UCR4:8000
UFCR:801
USR1:2040
USR2:5008
UBIR:0
UBMR:0
UBRC:4
UTS:60
--------serial_8250_startup:359---------
UCR1:1
UCR2:6027
UCR3:704
UCR4:8000
UFCR:801
USR1:2040
USR2:5008
UBIR:0
UBMR:0
UBRC:4
UTS:60
--------serial_8250_startup:371---------
UCR1:1
UCR2:6027
UCR3:704
UCR4:3810
UFCR:801
USR1:2040
USR2:5008
UBIR:0
UBMR:0
UBRC:4
UTS:60
--------serial_8250_startup:377---------
UCR1:1
UCR2:6027
UCR3:704
UCR4:3810
UFCR:1301
USR1:2040
USR2:5008
UBIR:0
UBMR:0
UBRC:4
UTS:60
--------serial_8250_startup:382---------
UCR1:1
UCR2:6027
UCR3:704
UCR4:3810
UFCR:1301
USR1:2040
USR2:5008
UBIR:bf
UBMR:0
UBRC:4
UTS:60
--------serial_8250_startup:386---------
UCR1:1
UCR2:6027
UCR3:704
UCR4:3810
UFCR:1301
USR1:2040
USR2:5008
UBIR:bf
UBMR:1be5
UBRC:4
UTS:60
--------serial_8250_startup:390---------
UCR1:601
UCR2:6027
UCR3:704
UCR4:3810
UFCR:1301
USR1:2040
USR2:5008
UBIR:bf
UBMR:1be5
UBRC:4
UTS:60
--------serial_8250_startup:394---------
--------serial_8250_probe:628---------
input: elan-touch as /devices/virtual/input/input1
fsl-usb2-udc fsl-usb2-udc: Plug Contact = 1
--------serial_8250_probe:650---------
Hanwon Serial tablet driver!
using rtc device, snvs_rtc, for alarms
snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0
i2c /dev entries driver
Linux video capture interface: v2.00
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v1.1.0)
i2c-core: driver [mag3110] using legacy suspend method
i2c-core: driver [mag3110] using legacy resume method
fsl-usb2-udc fsl-usb2-udc: It is a stardard downstream port
charger is SDP
imx6 usb charger online:1
-----------tps65185_sensor_probe---------
imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)
device-mapper: uevent: version 1.0.3
device-mapper: ioctl: 4.20.0-ioctl (2011-02-02) initialised: dm-devel@redhat.com
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci [sdhci_add_host()]: Disabling ADMA as it is marked broken
sdhci [sdhci_add_host()]: mmc0: Auto-CMD23 unavailable
sdhci: =========== REGISTER DUMP (mmc0)===========
sdhci: Sys addr: 0x00000000 | Version: 0x00000202
sdhci: Blk size: 0x00000200 | Blk cnt: 0x00000001
sdhci: Argument: 0x00000000 | Trn mode: 0x00000000
sdhci: Present: 0xfff98088 | Host ctl: 0x00000020
sdhci: Power: 0x0000000d | Blk gap: 0x00000000
sdhci: Wake-up: 0x00000000 | Clock: 0x00000018
sdhci: Timeout: 0x00000000 | Int stat: 0x00000000
sdhci: Int enab: 0x007f0003 | Sig enab: 0x007f0003
sdhci: AC12 err: 0x00000000 | Slot int: 0x00000202
sdhci: Caps: 0x07ebb407 | Caps_1: 0x0000b407
sdhci: Cmd: 0x00000d1a | Max curr: 0x00ffffff
sdhci: Host ctl2: 0x00000000
sdhci: ===========================================
mmc0: clock 0Hz busmode 1 powermode 0 cs 0 Vdd 0 width 0 timing 0
mmc0: mmc_rescan_try_freq: trying to init card at 400000 Hz
mmc0: clock 0Hz busmode 1 powermode 1 cs 0 Vdd 21 width 0 timing 0
mmc0: SDHCI controller on platform [sdhci-esdhc-imx.0] using DMA
android_work: did not send uevent (0 0 (null))
Galcore version 4.6.9.9754
Thermal calibration data is 0x5945175f
mmc0: clock 400000Hz busmode 1 powermode 2 cs 0 Vdd 21 width 0 timing 0
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
Thermal sensor with ratio = 185
Anatop Thermal registered as thermal_zone0
anatop_thermal_probe: default cooling device is cpufreq!
mmc0: starting CMD52 arg 00000c00 flags 00000195
android_usb gadget: unknown class-specific control req 80.06 v0100 i0000 l64
USB Gadget resume begins
fsl_udc_resume, Wait for wakeup thread finishes
usbcore: registered new interface driver usbhid
android_work: sent uevent USB_STATE=CONNECTED
usbhid: USB HID core driver
android_work: sent uevent USB_STATE=DISCONNECTED
logger: created 256K log 'log_main'
logger: created 256K log 'log_events'
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000
mmc0: req done (CMD52): -110: 00000000 00000000 00000000 00000000
mmc0: starting CMD52 arg 80000c08 flags 00000195
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000
mmc0: req done (CMD52): -110: 00000000 00000000 00000000 00000000
mmc0: clock 400000Hz busmode 1 powermode 2 cs 1 Vdd 21 width 0 timing 0
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
logger: created 256K log 'log_radio'
logger: created 256K log 'log_system'
usbcore: registered new interface driver snd-usb-audio
mmc0: starting CMD0 arg 00000000 flags 000000c0
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD0): 0: 00000000 00000000 00000000 00000000
mmc0: clock 400000Hz busmode 1 powermode 2 cs 0 Vdd 21 width 0 timing 0
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
android_usb gadget: unknown class-specific control req 80.06 v0100 i0000 l18
android_work: sent uevent USB_STATE=CONNECTED
android_usb gadget: unknown class-specific control req 80.06 v0200 i0000 l255
ALSA device list:
No soundcards found.
u32 classifier
Actions configured
Netfilter messages via NETLINK v0.30.
nf_conntrack version 0.5.0 (16384 buckets, 65536 max)
ctnetlink v0.93: registering with nfnetlink.
NF_TPROXY: Transparent proxy support initialized, version 4.1.0
NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.
mmc0: starting CMD8 arg 000001aa flags 000002f5
xt_time: kernel timezone is -0000
ip_tables: (C) 2000-2006 Netfilter Core Team
arp_tables: (C) 2002 David S. Miller
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000
mmc0: req done (CMD8): -110: 00000000 00000000 00000000 00000000
mmc0: starting CMD5 arg 00000000 flags 000002e1
TCP cubic registered
Initializing XFRM netlink socket
NET: Registered protocol family 10
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000
mmc0: req failed (CMD5): -110, retrying...
Mobile IPv6
ip6_tables: (C) 2000-2006 Netfilter Core Team
NET: Registered protocol family 17
NET: Registered protocol family 15
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000
mmc0: req failed (CMD5): -110, retrying...
lib80211: common routines for IEEE802.11 drivers
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000
mmc0: req failed (CMD5): -110, retrying...
lib80211_crypt: registered algorithm 'NULL'
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000
mmc0: req done (CMD5): -110: 00000000 00000000 00000000 00000000
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
lib80211_crypt: registered algorithm 'WEP'
lib80211_crypt: registered algorithm 'CCMP'
android_work: sent uevent USB_STATE=DISCONNECTED
lib80211_crypt: registered algorithm 'TKIP'
mmc0: starting CMD55 arg 00000000 flags 000000f5
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000
mmc0: req done (CMD55): -110: 00000000 00000000 00000000 00000000
Bus freq driver module loaded
Bus freq driver Enabled
mxc_dvfs_core_probe
mmc0: starting CMD55 arg 00000000 flags 000000f5
DVFS driver module loaded
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000
android_usb gadget: unknown class-specific control req 80.06 v0100 i0000 l64
mmc0: req done (CMD55): -110: 00000000 00000000 00000000 00000000
android_work: did not send uevent (0 0 (null))
mmc0: starting CMD55 arg 00000000 flags 000000f5
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000
mmc0: req done (CMD55): -110: 00000000 00000000 00000000 00000000
mmc0: starting CMD55 arg 00000000 flags 000000f5
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000
mmc0: req done (CMD55): -110: 00000000 00000000 00000000 00000000
mmc0: starting CMD1 arg 00000000 flags 000000e1
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD1): 0: 00ff8080 00000000 00000000 00000000
mmc0: clock 400000Hz busmode 1 powermode 2 cs 0 Vdd 7 width 0 timing 0
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
MXCFB_SET_WAVEFORM_MODES:4018462b
MXCFB_SET_TEMPERATURE:4004462c
MXCFB_SET_AUTO_UPDATE_MODE:4004462d
MXCFB_SEND_UPDATE:4040462e
MXCFB_WAIT_FOR_UPDATE_COMPLETE:c008462f
MXCFB_SET_PWRDOWN_DELAY:40044630
MXCFB_GET_PWRDOWN_DELAY:80044631
mmc0: clock 400000Hz busmode 1 powermode 2 cs 0 Vdd 7 width 0 timing 0
android_usb gadget: unknown class-specific control req 80.06 v0100 i0000 l18
MXCFB_SET_UPDATE_SCHEME:40044632
android_usb gadget: unknown class-specific control req 80.06 v0200 i0000 l255
android_work: sent uevent USB_STATE=CONNECTED
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
MXCFB_GET_WORK_BUFFER:c0044634
imx_epdc_fb imx_epdc_fb: ---resolution 1200x825, bpp 16
imx_epdc_fb imx_epdc_fb: ---xres: 1216, yres:896, max:1089536
imx_epdc_fb imx_epdc_fb: ---xres: 832, yres:1280, max:1064960
imx_epdc_fb imx_epdc_fb: ---buf_size allocate: 2179072, x_mem_size:0
mmc0: clock 400000Hz busmode 1 powermode 2 cs 1 Vdd 7 width 0 timing 0
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
imx_epdc_fb imx_epdc_fb: ---map_size allocate: 6537216, num_screen:3
imx_epdc_fb imx_epdc_fb: ---screen_base allocated at ff400000:0xff400000, 0xa6800000
mmc0: starting CMD0 arg 00000000 flags 000000c0
imx_epdc_fb imx_epdc_fb: ---EPDC version = 21
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD0): 0: 00000000 00000000 00000000 00000000
mmc0: clock 400000Hz busmode 1 powermode 2 cs 0 Vdd 7 width 0 timing 0
imx_epdc_fb imx_epdc_fb: ---upd_list[0]:0xe60019a0, size: 20
android_work: sent uevent USB_STATE=DISCONNECTED
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
imx_epdc_fb imx_epdc_fb: ---upd_list[1]:0xe60019e0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[2]:0xe6001a00, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[3]:0xe6001a20, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[4]:0xe6001a40, size: 20
mmc0: starting CMD1 arg 40000080 flags 000000e1
imx_epdc_fb imx_epdc_fb: ---upd_list[5]:0xe60019c0, size: 20
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD1): 0: 00ff8080 00000000 00000000 00000000
imx_epdc_fb imx_epdc_fb: ---upd_list[6]:0xe60017c0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[7]:0xe6001a60, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[8]:0xe6001a80, size: 20
android_usb gadget: unknown class-specific control req 80.06 v0100 i0000 l64
mmc0: starting CMD1 arg 40000080 flags 000000e1
imx_epdc_fb imx_epdc_fb: ---upd_list[9]:0xe6001ac0, size: 20
android_work: sent uevent USB_STATE=CONNECTED
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD1): 0: c0ff8080 00000000 00000000 00000000
mmc0: starting CMD2 arg 00000000 flags 00000067
imx_epdc_fb imx_epdc_fb: ---upd_list[10]:0xe6001b00, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[11]:0xe6001b20, size: 20
android_work: sent uevent USB_STATE=DISCONNECTED
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD2): 0: 11010030 30384737 300088b9 2cb94200
mmc0: starting CMD3 arg 00010000 flags 00000015
imx_epdc_fb imx_epdc_fb: ---upd_list[12]:0xe6001ae0, size: 20
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD3): 0: 00000500 00000000 00000000 00000000
mmc0: clock 400000Hz busmode 2 powermode 2 cs 0 Vdd 7 width 0 timing 0
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
imx_epdc_fb imx_epdc_fb: ---upd_list[13]:0xe6001aa0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[14]:0xe6001b60, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[15]:0xe6001b40, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[16]:0xe6001b80, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[17]:0xe6001ba0, size: 20
android_usb gadget: unknown class-specific control req 80.06 v0100 i0000 l18
mmc0: starting CMD9 arg 00010000 flags 00000007
android_usb gadget: unknown class-specific control req 80.06 v0200 i0000 l255
android_work: sent uevent USB_STATE=CONNECTED
imx_epdc_fb imx_epdc_fb: ---upd_list[18]:0xe6001c00, size: 20
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD9): 0: d0270032 0f5903ff ffffffe7 86400000
mmc0: starting CMD7 arg 00010000 flags 00000015
imx_epdc_fb imx_epdc_fb: ---upd_list[19]:0xe6001c20, size: 20
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD7): 0: 00000700 00000000 00000000 00000000
mmc0: starting CMD8 arg 00000000 flags 000000b5
mmc0: blksz 512 blocks 1 flags 00000200 tsac 150 ms nsac 0
imx_epdc_fb imx_epdc_fb: ---upd_list[20]:0xe6001c40, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[21]:0xe6001c60, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[22]:0xe6001be0, size: 20
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
imx_epdc_fb imx_epdc_fb: ---upd_list[23]:0xe6001bc0, size: 20
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x0000000a
sdhci [sdhci_data_irq()]: mmc0: DMA base 0xa6486200, transferred 0x079e00 bytes, next 0xa6500000
mmc0: req done (CMD8): 0: 00000900 00000000 00000000 00000000
mmc0: 512 bytes transferred: 0
---mmc_init_card--- 3!/n
mmc0: starting CMD6 arg 03b90101 flags 0000049d
imx_epdc_fb imx_epdc_fb: ---upd_list[24]:0xe6001c80, size: 20
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD6): 0: 00000800 00000000 00000000 00000000
mmc0: starting CMD13 arg 00010000 flags 00000195
imx_epdc_fb imx_epdc_fb: ---upd_list[25]:0xe6001ca0, size: 20
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD13): 0: 00000900 00000000 00000000 00000000
mmc0: clock 400000Hz busmode 2 powermode 2 cs 0 Vdd 7 width 0 timing 1
imx_epdc_fb imx_epdc_fb: ---upd_list[26]:0xe6001cc0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[27]:0xe6001ce0, size: 20
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
sdhci sdhci-esdhc-imx.0: desired SD clock: 400000, actual: 375000
imx_epdc_fb imx_epdc_fb: ---upd_list[28]:0xe6001d00, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[29]:0xe6001d20, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[30]:0xe6001d40, size: 20
mmc0: clock 52000000Hz busmode 2 powermode 2 cs 0 Vdd 7 width 0 timing 1
sdhci sdhci-esdhc-imx.0: desired SD clock: 52000000, actual: 45000000
sdhci sdhci-esdhc-imx.0: desired SD clock: 52000000, actual: 45000000
sdhci sdhci-esdhc-imx.0: desired SD clock: 52000000, actual: 45000000
sdhci sdhci-esdhc-imx.0: desired SD clock: 52000000, actual: 45000000
imx_epdc_fb imx_epdc_fb: ---upd_list[31]:0xe6001d60, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[32]:0xe6001d80, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[33]:0xe6001da0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[34]:0xe6001dc0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[35]:0xe6001de0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[36]:0xe6001e00, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[37]:0xe6001e20, size: 20
mmc0: starting CMD8 arg 00000000 flags 000000b5
mmc0: blksz 512 blocks 1 flags 00000200 tsac 150 ms nsac 0
imx_epdc_fb imx_epdc_fb: ---upd_list[38]:0xe6001e40, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[39]:0xe6001e60, size: 20
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x0000000a
sdhci [sdhci_data_irq()]: mmc0: DMA base 0xa6486000, transferred 0x07a000 bytes, next 0xa6500000
mmc0: req done (CMD8): 0: 00000900 00000000 00000000 00000000
mmc0: 512 bytes transferred: 0
---mmc_select_powerclass--- !/n
mmc0: starting CMD6 arg 03bb0a01 flags 0000049d
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD6): 0: 00000800 00000000 00000000 00000000
mmc0: starting CMD13 arg 00010000 flags 00000195
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD13): 0: 00000900 00000000 00000000 00000000
imx_epdc_fb imx_epdc_fb: ---upd_list[40]:0xe6001e80, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[41]:0xe6001ea0, size: 20
---mmc_init_card--- 4!/n
mmc0: starting CMD6 arg 03b70201 flags 0000049d
imx_epdc_fb imx_epdc_fb: ---upd_list[42]:0xe6001ec0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[43]:0xe6001ee0, size: 20
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD6): 0: 00000800 00000000 00000000 00000000
mmc0: starting CMD13 arg 00010000 flags 00000195
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD13): 0: 00000900 00000000 00000000 00000000
mmc0: clock 52000000Hz busmode 2 powermode 2 cs 0 Vdd 7 width 3 timing 1
sdhci sdhci-esdhc-imx.0: desired SD clock: 52000000, actual: 45000000
sdhci sdhci-esdhc-imx.0: desired SD clock: 52000000, actual: 45000000
sdhci sdhci-esdhc-imx.0: desired SD clock: 52000000, actual: 45000000
imx_epdc_fb imx_epdc_fb: ---upd_list[44]:0xe6001f00, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[45]:0xe6001f20, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[46]:0xe6001f40, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[47]:0xe6001f60, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[48]:0xe6001f80, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[49]:0xe6001fa0, size: 20
mmc0: starting CMD8 arg 00000000 flags 000000b5
mmc0: blksz 512 blocks 1 flags 00000200 tsac 150 ms nsac 0
imx_epdc_fb imx_epdc_fb: ---upd_list[50]:0xe6001fc0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[51]:0xe6001fe0, size: 20
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x0000000a
sdhci [sdhci_data_irq()]: mmc0: DMA base 0xa6486000, transferred 0x07a000 bytes, next 0xa6500000
mmc0: req done (CMD8): 0: 00000900 00000000 00000000 00000000
mmc0: 512 bytes transferred: 0
mmc0: starting CMD8 arg 00000000 flags 000000b5
imx_epdc_fb imx_epdc_fb: ---upd_list[52]:0xe60081e0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[53]:0xe6008200, size: 20
mmc0: blksz 512 blocks 1 flags 00000200 tsac 150 ms nsac 0
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x0000000a
sdhci [sdhci_data_irq()]: mmc0: DMA base 0xa6486000, transferred 0x07a000 bytes, next 0xa6500000
mmc0: req done (CMD8): 0: 00000900 00000000 00000000 00000000
mmc0: 512 bytes transferred: 0
---mmc_select_powerclass--- !/n
mmc0: starting CMD6 arg 03bb0a01 flags 0000049d
imx_epdc_fb imx_epdc_fb: ---upd_list[54]:0xe6008220, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[55]:0xe6008240, size: 20
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD6): 0: 00000800 00000000 00000000 00000000
mmc0: starting CMD13 arg 00010000 flags 00000195
imx_epdc_fb imx_epdc_fb: ---upd_list[56]:0xe6008260, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[57]:0xe6008280, size: 20
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD13): 0: 00000900 00000000 00000000 00000000
---mmc_init_card--- 4!/n
mmc0: starting CMD6 arg 03b70601 flags 0000049d
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD6): 0: 00000800 00000000 00000000 00000000
mmc0: starting CMD13 arg 00010000 flags 00000195
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD13): 0: 00000900 00000000 00000000 00000000
mmc0: clock 52000000Hz busmode 2 powermode 2 cs 0 Vdd 7 width 3 timing 5
imx_epdc_fb imx_epdc_fb: ---upd_list[58]:0xe60082a0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[59]:0xe60082c0, size: 20
sdhci sdhci-esdhc-imx.0: desired SD clock: 52000000, actual: 45000000
sdhci sdhci-esdhc-imx.0: desired SD clock: 52000000, actual: 45000000
sdhci sdhci-esdhc-imx.0: desired SD clock: 52000000, actual: 45000000
imx_epdc_fb imx_epdc_fb: ---upd_list[60]:0xe60082e0, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[61]:0xe640c980, size: 20
imx_epdc_fb imx_epdc_fb: ---upd_list[62]:0xe640c960, size: 20
mmc0: clock 52000000Hz busmode 2 powermode 2 cs 0 Vdd 7 width 3 timing 5
sdhci sdhci-esdhc-imx.0: desired SD clock: 52000000, actual: 45000000
sdhci sdhci-esdhc-imx.0: desired SD clock: 52000000, actual: 45000000
sdhci sdhci-esdhc-imx.0: desired SD clock: 52000000, actual: 45000000
imx_epdc_fb imx_epdc_fb: ---upd_list[63]:0xe6ffe940, size: 20
imx_epdc_fb imx_epdc_fb: ---size of void*:4, sizeof dma:4, max_num_buffers:2
imx_epdc_fb imx_epdc_fb: ---upd_buf0 virt:0xE6FFE920, phys:0xE6FFE900
imx_epdc_fb imx_epdc_fb: ---upd_buf allocated 1089536 bytes virt:0xE7000000, phys:0xA7000000, PHYS_OFFSET:80000000
mmc0: new high speed DDR MMC card at address 0001
imx_epdc_fb imx_epdc_fb: ---upd_buf allocated 1089536 bytes virt:0xE7200000, phys:0xA7200000, PHYS_OFFSET:80000000
mmcblk0: mmc0:0001 008G70 7.28 GiB
mmcblk0boot0: mmc0:0001 008G70 partition 1 4.00 MiB
imx_epdc_fb imx_epdc_fb: ---copy 0xFF100000,phys_copy:0xA7800000, working:0xFEF00000, working_phys0xa7600000,work size:1980000
mmcblk0boot1: mmc0:0001 008G70 partition 2 4.00 MiB
submit_bh 1
---mmc_blk_rw_rq_prep-- !
mmc0: starting CMD18 arg 00000000 flags 000000b5
mmc0: blksz 512 blocks 8 flags 00000200 tsac 150 ms nsac 0
submit_bh 2
submit_bh 3
submit_bh 4
mmc0: CMD12 arg 00000000 flags 0000049d
imx_epdc_fb imx_epdc_fb: --num_luts:64 -lut:0xE63FC1E0, size u32*: 4
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x0000000a
sdhci [sdhci_data_irq()]: mmc0: DMA base 0xa6500000, transferred 0x080000 bytes, next 0xa6580000
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD18): 0: 00000900 00000000 00000000 00000000
mmc0: 4096 bytes transferred: 0
mmc0: (CMD12): 0: 00000b00 00000000 00000000 00000000
submit_bh 1
---mmc_blk_rw_rq_prep-- !
submit_bh 2
submit_bh 3
submit_bh 4
mmc0: starting CMD18 arg 0001e000 flags 000000b5
mmc0: blksz 512 blocks 8 flags 00000200 tsac 150 ms nsac 0
mmc0: CMD12 arg 00000000 flags 0000049d
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x0000000a
sdhci [sdhci_data_irq()]: mmc0: DMA base 0xa6e80000, transferred 0x080000 bytes, next 0xa6f00000
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD18): 0: 00000900 00000000 00000000 00000000
mmc0: 4096 bytes transferred: 0
mmc0: (CMD12): 0: 00000b00 00000000 00000000 00000000
submit_bh 1
---mmc_blk_rw_rq_prep-- !
mmc0: starting CMD18 arg 0011e000 flags 000000b5
submit_bh 2
submit_bh 3
submit_bh 4
imx_epdc_fb imx_epdc_fb: ---lut_map:0xe63fc0e0
mmc0: blksz 512 blocks 8 flags 00000200 tsac 150 ms nsac 0
mmc0: CMD12 arg 00000000 flags 0000049d
-----tps65185_vcom_set_voltage---
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x0000000a
sdhci [sdhci_data_irq()]: mmc0: DMA base 0xa6500000, transferred 0x080000 bytes, next 0xa6580000
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD18): 0: 00000900 00000000 00000000 00000000
mmc0: 4096 bytes transferred: 0
mmc0: (CMD12): 0: 00000b00 00000000 00000000 00000000
usb usb1: usb_suspend_both: status 0
hub 2-0:1.0: usb_suspend_interface: status 0
ehci_fsl_bus_suspend begins, Host 1
submit_bh 1
submit_bh 2
submit_bh 3
---mmc_blk_rw_rq_prep-- !
submit_bh 4
mmc0: starting CMD18 arg 0021e000 flags 000000b5
mmc0: blksz 512 blocks 8 flags 00000200 tsac 150 ms nsac 0
mmc0: CMD12 arg 00000000 flags 0000049d
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x0000000a
sdhci [sdhci_data_irq()]: mmc0: DMA base 0xa6500000, transferred 0x080000 bytes, next 0xa6580000
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD18): 0: 00000900 00000000 00000000 00000000
mmc0: 4096 bytes transferred: 0
mmc0: (CMD12): 0: 00000b00 00000000 00000000 00000000
submit_bh 1
---mmc_blk_rw_rq_prep-- !
mmc0: starting CMD18 arg 00222000 flags 000000b5
mmc0: blksz 512 blocks 8 flags 00000200 tsac 150 ms nsac 0
submit_bh 2
submit_bh 3
submit_bh 4
ehci_fsl_bus_suspend ends, Host 1
usb usb2: usb_suspend_device: status 0
usb usb2: usb_suspend_both: status 0
mmc0: CMD12 arg 00000000 flags 0000049d
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x0000000a
sdhci [sdhci_data_irq()]: mmc0: DMA base 0xa6e80000, transferred 0x080000 bytes, next 0xa6f00000
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD18): 0: 00000900 00000000 00000000 00000000
mmc0: 4096 bytes transferred: 0
mmc0: (CMD12): 0: 00000b00 00000000 00000000 00000000
mmcblk0: p1 p2 p3 < p5 p6 p7 p8 > p4
mmcblk0: p4 size 13017088 extends beyond EOD, truncated
submit_bh 1
---mmc_blk_part_switch--- !
mmc_switch part_config = 74; part_time = 100
mmc0: starting CMD6 arg 03b34a01 flags 0000049d
submit_bh 2
submit_bh 3
submit_bh 4
tps65185 0-0068: Vcom set : -1400 mV
-----tps65185_vcom_is_enabled---
-----tps65185_display_is_enable---
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD6): 0: 00000800 00000000 00000000 00000000
mmc0: starting CMD13 arg 00010000 flags 00000195
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD13): 0: 00000900 00000000 00000000 00000000
---mmc_blk_rw_rq_prep-- !
mmc0: starting CMD18 arg 00000000 flags 000000b5
regulator_init_complete: PFUZE100_VGEN6: incomplete constraints, leaving on
mmc0: blksz 512 blocks 8 flags 00000200 tsac 150 ms nsac 0
mmc0: CMD12 arg 00000000 flags 0000049d
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x0000000a
sdhci [sdhci_data_irq()]: mmc0: DMA base 0xa7500000, transferred 0x080000 bytes, next 0xa7580000
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD18): 0: 00000900 00000000 00000000 00000000
mmc0: 4096 bytes transferred: 0
mmc0: (CMD12): 0: 00000b00 00000000 00000000 00000000
submit_bh 1
submit_bh 2
submit_bh 3
submit_bh 4
---mmc_blk_rw_rq_prep-- !
regulator_init_complete: PFUZE100_VGEN5: incomplete constraints, leaving on
mmc0: starting CMD18 arg 00000018 flags 000000b5
mmc0: blksz 512 blocks 8 flags 00000200 tsac 150 ms nsac 0
mmc0: CMD12 arg 00000000 flags 0000049d
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x0000000a
sdhci [sdhci_data_irq()]: mmc0: DMA base 0xa7500000, transferred 0x080000 bytes, next 0xa7580000
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD18): 0: 00000900 00000000 00000000 00000000
mmc0: 4096 bytes transferred: 0
mmc0: (CMD12): 0: 00000b00 00000000 00000000 00000000
mmcblk0boot1: unknown partition table
regulator_init_complete: PFUZE100_VGEN3: incomplete constraints, leaving on
submit_bh 1
---mmc_blk_part_switch--- !
submit_bh 2
submit_bh 3
submit_bh 4
mmc_switch part_config = 73; part_time = 100
mmc0: starting CMD6 arg 03b34901 flags 0000049d
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD6): 0: 00000800 00000000 00000000 00000000
regulator_init_complete: SPKVDD: incomplete constraints, leaving on
mmc0: starting CMD13 arg 00010000 flags 00000195
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD13): 0: 00000900 00000000 00000000 00000000
---mmc_blk_rw_rq_prep-- !
mmc0: starting CMD18 arg 00000000 flags 000000b5
snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 08:20:13 UTC (30013)
mmc0: blksz 512 blocks 8 flags 00000200 tsac 150 ms nsac 0
mmc0: CMD12 arg 00000000 flags 0000049d
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x0000000a
sdhci [sdhci_data_irq()]: mmc0: DMA base 0xa7400000, transferred 0x080000 bytes, next 0xa7480000
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD18): 0: 00000900 00000000 00000000 00000000
mmc0: 4096 bytes transferred: 0
mmc0: (CMD12): 0: 00000b00 00000000 00000000 00000000
submit_bh 1
---mmc_blk_rw_rq_prep-- !
submit_bh 2
submit_bh 3
submit_bh 4
mmc0: starting CMD18 arg 00000018 flags 000000b5
mmc0: blksz 512 blocks 8 flags 00000200 tsac 150 ms nsac 0
Freeing init memory: 192K
do_mount 1
do_mount 2
do_mount 3
do_mount 4
do_mount 5
do_mount 6
do_new_mount 1 type = tmpfs,flags = 0,mnt_flags = 33, name = tmpfs
mmc0: CMD12 arg 00000000 flags 0000049d
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x0000000a
sdhci [sdhci_data_irq()]: mmc0: DMA base 0xa6580000, transferred 0x080000 bytes, next 0xa6600000
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00000001
mmc0: req done (CMD18): 0: 00000900 00000000 00000000 00000000
mmc0: 4096 bytes transferred: 0
mmc0: (CMD12): 0: 00000b00 00000000 00000000 00000000
do_new_mount 2
do_new_mount 3
do_kern_mount1
vfs_kern_mount 1
vfs_kern_mount 2
vfs_kern_mount 3
mount_fs 1
mount_fs 2
mount_fs 3
mount_fs 4
mount_fs 5
mount_fs 6
mount_fs 7
mount_fs 8
vfs_kern_mount 5
do_kern_mount3
do_new_mount 4
do_new_mount 5 err = 0
do_mount 11 retval = 0
do_mount 1
do_mount 2
do_mount 3
do_mount 4
do_mount 5
do_mount 6
do_new_mount 1 type = devpts,flags = 0,mnt_flags = 32, name = devpts
mmcblk0boot0: unknown partition table
do_new_mount 2
do_new_mount 3
do_kern_mount1
vfs_kern_mount 1
vfs_kern_mount 2
vfs_kern_mount 3
mount_fs 1
mount_fs 3
mount_fs 4
mount_fs 5
mount_fs 6
mount_fs 7
mount_fs 8
vfs_kern_mount 5
do_kern_mount3
do_new_mount 4
do_new_mount 5 err = 0
do_mount 11 retval = 0
do_mount 1
do_mount 2
do_mount 3
do_mount 4
do_mount 5
do_mount 6
do_new_mount 1 type = proc,flags = 0,mnt_flags = 32, name = proc
do_new_mount 2
do_new_mount 3
do_kern_mount1
vfs_kern_mount 1
vfs_kern_mount 2
vfs_kern_mount 3
mount_fs 1
mount_fs 3
mount_fs 4
mount_fs 5
mount_fs 6
mount_fs 7
mount_fs 8
vfs_kern_mount 5
do_kern_mount3
do_new_mount 4
do_new_mount 5 err = 0
do_mount 11 retval = 0
do_mount 1
do_mount 2
do_mount 3
do_mount 4
do_mount 5
do_mount 6
do_new_mount 1 type = sysfs,flags = 0,mnt_flags = 32, name = sysfs
do_new_mount 2
do_new_mount 3
do_kern_mount1
vfs_kern_mount 1
vfs_kern_mount 2
vfs_kern_mount 3
mount_fs 1
mount_fs 3
mount_fs 4
mount_fs 5
mount_fs 6
mount_fs 7
mount_fs 8
vfs_kern_mount 5
do_kern_mount3
do_new_mount 4
do_new_mount 5 err = 0
do_mount 11 retval = 0
init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead.
rt_fg_get_property: FG_SOC=1020, SYS_SOC=100
init: /dev/hw_random not found
keychord: using input dev imx-keypad for fevent
do_mount 1
do_mount 2
do_mount 3
do_mount 4
do_mount 5
do_mount 6
do_new_mount 1 type = cgroup,flags = 0,mnt_flags = 32, name = none
do_new_mount 2
do_new_mount 3
do_kern_mount1
vfs_kern_mount 1
vfs_kern_mount 2
vfs_kern_mount 3
mount_fs 1
mount_fs 2
mount_fs 3
mount_fs 10
mount_fs 11
vfs_kern_mount 4
do_kern_mount3
do_mount 11 retval = -2
do_mount 1
do_mount 2
do_mount 3
do_mount 4
do_mount 5
do_mount 6
do_new_mount 1 type = tmpfs,flags = 0,mnt_flags = 32, name = none
do_new_mount 2
do_new_mount 3
do_kern_mount1
vfs_kern_mount 1
vfs_kern_mount 2
vfs_kern_mount 3
mount_fs 1
mount_fs 2
mount_fs 3
mount_fs 4
mount_fs 5
mount_fs 6
mount_fs 7
mount_fs 8
vfs_kern_mount 5
do_kern_mount3
do_new_mount 4
do_new_mount 5 err = 0
do_mount 11 retval = 0
do_mount 1
do_mount 2
do_mount 3
do_mount 4
do_mount 5
do_mount 6
do_new_mount 1 type = cgroup,flags = 0,mnt_flags = 32, name = none
do_new_mount 2
do_new_mount 3
do_kern_mount1
vfs_kern_mount 1
vfs_kern_mount 2
vfs_kern_mount 3
mount_fs 1
mount_fs 2
mount_fs 3
mount_fs 10
mount_fs 11
vfs_kern_mount 4
do_kern_mount3
do_mount 11 retval = -2
do_mount 1
do_mount 2
do_mount 3
do_mount 4
do_mount 5
do_mount 6
do_new_mount 1 type = tmpfs,flags = 0,mnt_flags = 32, name = tmpfs
do_new_mount 2
do_new_mount 3
do_kern_mount1
vfs_kern_mount 1
vfs_kern_mount 2
vfs_kern_mount 3
mount_fs 1
mount_fs 2
mount_fs 3
mount_fs 4
mount_fs 5
mount_fs 6
mount_fs 7
mount_fs 8
vfs_kern_mount 5
do_kern_mount3
do_new_mount 4
do_new_mount 5 err = 0
do_mount 11 retval = 0
do_mount 1
do_mount 2
do_mount 3
do_mount 4
do_mount 5
do_mount 6
do_new_mount 1 type = tmpfs,flags = 0,mnt_flags = 32, name = tmpfs
do_new_mount 2
do_new_mount 3
do_kern_mount1
vfs_kern_mount 1
vfs_kern_mount 2
vfs_kern_mount 3
mount_fs 1
mount_fs 2
mount_fs 3
mount_fs 4
mount_fs 5
mount_fs 6
mount_fs 7
mount_fs 8
vfs_kern_mount 5
do_kern_mount3
do_new_mount 4
do_new_mount 5 err = 0
do_mount 11 retval = 0
do_mount 1
do_mount 2
do_mount 3
do_mount 4
do_mount 5
do_mount 6
do_new_mount 1 type = tmpfs,flags = 0,mnt_flags = 32, name = tmpfs
do_new_mount 2
do_new_mount 3
do_kern_mount1
vfs_kern_mount 1
vfs_kern_mount 2
vfs_kern_mount 3
mount_fs 1
mount_fs 2
mount_fs 3
mount_fs 4
mount_fs 5
mount_fs 6
mount_fs 7
mount_fs 8
vfs_kern_mount 5
do_kern_mount3
do_new_mount 4
do_new_mount 5 err = 0
do_mount 11 retval = 0
do_mount 1
do_mount 2
do_mount 3
do_mount 4
do_mount 5
do_mount 6
do_new_mount 1 type = tmpfs,flags = 0,mnt_flags = 32, name = tmpfs
do_new_mount 2
do_new_mount 3
do_kern_mount1
vfs_kern_mount 1
vfs_kern_mount 2
vfs_kern_mount 3
mount_fs 1
mount_fs 2
mount_fs 3
mount_fs 4
mount_fs 5
mount_fs 6
mount_fs 7
mount_fs 8
vfs_kern_mount 5
do_kern_mount3
do_new_mount 4
do_new_mount 5 err = 0
do_mount 11 retval = 0
do_mount 1
do_mount 2
do_mount 3
do_mount 4
do_mount 5
do_mount 6
do_new_mount 1 type = cgroup,flags = 0,mnt_flags = 32, name = none
do_new_mount 2
do_new_mount 3
do_kern_mount1
vfs_kern_mount 1
vfs_kern_mount 2
vfs_kern_mount 3
mount_fs 1
mount_fs 2
mount_fs 3
mount_fs 4
mount_fs 5
mount_fs 6
mount_fs 7
mount_fs 8
vfs_kern_mount 5
do_kern_mount3
do_new_mount 4
do_new_mount 5 err = 0
do_mount 11 retval = 0
do_mount 1
do_mount 2
do_mount 3
do_mount 4
do_mount 5
do_mount 6
do_new_mount 1 type = ext4,flags = 0,mnt_flags = 32, name = /dev/block/mmcblk0p5
do_new_mount 2
do_new_mount 3
do_kern_mount1
vfs_kern_mount 1
vfs_kern_mount 2
vfs_kern_mount 3
mount_fs 1
mount_fs 3
ext4_mount
mount_bdev 1
mount_bdev 2
mount_bdev 3
mount_bdev 4
mount_bdev 6
ext4_fill_super 1
ext4_fill_super 2
ext4_fill_super 3
ext4_fill_super 4
ext4_fill_super 5
ext4_fill_super 7
ext4_fill_super 7.1
__bread block =400; size = 1
__getblk 1
__find_get_block 1
__find_get_block 3
__find_get_block 2
__getblk_slow 1
__find_get_block 1
__find_get_block 3
__find_get_block 2
__getblk_slow 2
__getblk_slow 3
__find_get_block 1
__find_get_block 3
__find_get_block 4
__find_get_block 2
__getblk 2
__bread 2
__bread_slow 1
__bread_slow 3
submit_bh 1
---mmc_blk_part_switch--- !
mmc_switch part_config = 72; part_time = 100
mmc0: starting CMD6 arg 03b34801 flags 0000049d
submit_bh 2
submit_bh 3
submit_bh 4
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000
mmc0: req failed (CMD6): -110, retrying...
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000
mmc0: req failed (CMD6): -110, retrying...
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000
mmc0: req failed (CMD6): -110, retrying...
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000
mmc0: req done (CMD6): -110: 00000000 00000000 00000000 00000000
---mmc_blk_part_switch--- !
mmc_switch part_config = 72; part_time = 100
mmc0: starting CMD6 arg 03b34801 flags 0000049d
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000
mmc0: req failed (CMD6): -110, retrying...
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000
mmc0: req failed (CMD6): -110, retrying...
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000
mmc0: req failed (CMD6): -110, retrying...
sdhci [sdhci_irq()]: *** mmc0 got interrupt: 0x00010000
mmc0: req done (CMD6): -110: 00000000 00000000 00000000 00000000
imx6 usb charger online:0
android_work: sent uevent USB_STATE=DISCONNECTED
fsl_gadget_disconnect_event: udc enter low power mode
ehci_fsl_bus_resume begins, Host 1
ehci_fsl_bus_resume ends, Host 1
usb usb2: usb_resume_device: status 0
解決済! 解決策の投稿を見る。
Hi,
everybody,i fixed this bug,
static const struct esdhc_platform_data mx6_evk_sd1_data __initconst = {
.always_present = 1,
.cd_gpio = -1,//MX6_BRD_SD1_CD,
.wp_gpio = -1,
.support_8bit = 1,
.keep_power_at_suspend = 1,
.delay_line = 0,
.support_18v = 1,
.platform_pad_change = plt_sd_pad_change,
.cd_type = ESDHC_CD_PERMANENT,
};
modify .support_18v = 1, to .support_18v = 0,
Hi,
everybody,i fixed this bug,
static const struct esdhc_platform_data mx6_evk_sd1_data __initconst = {
.always_present = 1,
.cd_gpio = -1,//MX6_BRD_SD1_CD,
.wp_gpio = -1,
.support_8bit = 1,
.keep_power_at_suspend = 1,
.delay_line = 0,
.support_18v = 1,
.platform_pad_change = plt_sd_pad_change,
.cd_type = ESDHC_CD_PERMANENT,
};
modify .support_18v = 1, to .support_18v = 0,
one can try to erase eMMC then program with mfg tools
sudo dd if=/dev/zero of =/dev/sdx
what is about linux, is it able to boot ?
Hi ,
i find one bbs https://community.nxp.com/message/473435#comment-477781 descripted same problem with my. Can you give me oen copy of the kernel v 3.10.17 code. thanks !!
my email is ramon20082001@163.com
please look at
i think maybe i should use this script <CMD state="Updater" type="push" body="$ dd if=/dev/zero of=/dev/mmcblk0 ">
but this can't execute sucessful
i didn’t try on linux。 but another anroid img can boot up normally,i don‘t have this img’s code。 so i think mmc driver code‘s problem is most probably。
Hi Ning
please use mfg tool for eMMC programming, as it automatically do all partition
formatting, refer to attached Android Guide sect.4.1.2 Downloading images with MFGTool
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov,
i use mfg tool all the time! But, the problem still there! Is there any other method?
Hi igorpadykov,
i don't understand your meaning . Did you mean i download images using wrong way?