build mfg frameware

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

build mfg frameware

Jump to solution
3,699 Views
wuhongbobo
Contributor II

你好,我参考Manufacturing Tool V2 Linux or Android Firmware Development Guide V2文档,编译mfg frameware,使用mfgtool重新下载os到emmc,,但是此时出现了错误
mfgtool卡在了access boot partition 1

console信息:
UTP: executing "dd if=/dev/zero of=/dev/mmcblk0 bs=512 seek=1536 count=16"

请问:

1 是我编译的mfg frameware不对吗,还是要使用ltib来编译呢?

2 如果用ltib编译,应该参考哪个文档呢?

Labels (1)
0 Kudos
Reply
1 Solution
3,447 Views
tootzoe
Contributor III

你这个问题应该是 内存 参数或者 layout 有问题, 内存工作不稳定 导致.

View solution in original post

5 Replies
3,447 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi hong wu,

Which BSP and board are you using?
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,447 Views
wuhongbobo
Contributor II

另外:

1,我使用I.MX6DQSDL DDR3 Script Aid V0.10.xlsx文件生成的inc脚本,载入V2.60版本的DDR Test Tool,开始后tool停留在如下画面,无法得到DQS 等配置。应该如何解决

pastedImage_1.png

2,我的板子emmc从8G扩大至16G,mfgtool里面的mksdcard-android.sh文件是否需要修改,如果需要该,有没有说明文档可以参考!

0 Kudos
Reply
3,448 Views
tootzoe
Contributor III

你这个问题应该是 内存 参数或者 layout 有问题, 内存工作不稳定 导致.

3,447 Views
wuhongbobo
Contributor II

谢谢,我让我们硬件工程师也检查一下。

0 Kudos
Reply
3,447 Views
wuhongbobo
Contributor II

android_jb4.3_1.0.0-ga

board is based on MX 6Quad SABRE-SD, just changed: DDR from 1G DDR2 to 2G ddr3;   and emmc from 8G to 16G

0 Kudos
Reply