booting through spi ...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

booting through spi ...

2,991 Views
aaa
Contributor I

i am able to write and read data into spi flash and i am working with imx 6q processor....i  wrote u-boot file into the spi leaving 4kb free region at the beginning of the spi flash.i also gave gave correct boot configurations but still not able to boot u-boot.Do i have to make any changes in the u-boot source say headers or something like that???

           thanx in advance

Labels (1)
0 Kudos
Reply
1 Reply

2,795 Views
igorpadykov
NXP Employee
NXP Employee

Hi aaaa

spi image ofset is 0x400 byte according to IMX6DQRM

Table 8-28. Image Vector Table Offset and Initial Load Region Size

For writing procedure please look at attached documents

sect.Flashing U-Boot on SPI-NOR From U-Boot.

Also one can look at MFG Tool  IMX_6DQ_MFG_TOOL :

ucl2.xml script how to program spi-nor in Linux.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply