boot up by tftpboot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

boot up by tftpboot

2,449 Views
mm2021
Contributor III

I'm debugging the i.MX 8M Mini board.

Now I can compile the kernel and get Image file. I put the Image file to SD card to replace the old one, the board can boot up to linux smoothly.
Now I'd like to get Image in ubbot by tftpboot.

As far as I know, in uboot, I can use the following command to load Image to ram:
tftp <addr in ram> Image

But how to set the address in ddr?

Thanks!

 

0 Kudos
Reply
2 Replies

2,420 Views
nxf63675
NXP TechSupport
NXP TechSupport

Hi @mm2021,

 

Please read the Linux user guide, chapter 4.4.1.2 Downloading an image to MMC/SD, there you will find how to do the configuration and the steps to follow.

https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf

 

For the loadaddr I think it is 0x40480000, also you could see this address if you, on U-boot write printenv and look for that address.

 

Hope this helps you.

Regards,

Israel.

0 Kudos
Reply

2,440 Views
mm2021
Contributor III

anybody can give some ideas?

0 Kudos
Reply