boot from nand

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

boot from nand

6,176 Views
enaud
Contributor III

Hi,

how is possible flash nand (with uboot.bin, uImage and rootfs) and start without SD but only from nand?

thanks

Labels (1)
0 Kudos
Reply
7 Replies

5,714 Views
enaud
Contributor III

QSB

0 Kudos
Reply

5,714 Views
KrishnaPavan
Contributor II

Is it QSB or SABRE or ARD or EVK etc etc.?

enaud said:

imx53

0 Kudos
Reply

5,714 Views
enaud
Contributor III

imx53

0 Kudos
Reply

5,714 Views
KrishnaPavan
Contributor II

Which board are you using?

0 Kudos
Reply

5,714 Views
DirkBehme
Contributor III

You might want to have a look to

http://imxcommunity.org/forum/topics/cannot-boot-from-nand

The discussion there is about the i.MX53 ARD board, but some parts might help for the QSB, too.

0 Kudos
Reply

5,714 Views
positron
Contributor I

Hello, Not only the hardware connection. You need to change the imximage.cfg (for u-boot) configurations to make it boot from NAND. If you are looking for a one-line answer on how to boot from NAND, I'd say "It is not that easy". You need to study the manual, patch in the IOMUX settings, write imximage.cfg, tweak the board file. Do it one step at a time.

0 Kudos
Reply

5,710 Views
jomeke
Contributor II

Hi Enaud,

you can find the information in the user manual under chapter 7.

I have made a summary in the Excel file attached.

Have a look

0 Kudos
Reply