bitbake fsl-image-gui errors out on do_configure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

bitbake fsl-image-gui errors out on do_configure

1,854 Views
bgoetz
Contributor I

Hello, I'm trying to get 'bitback fsl-image-gui' to work (attempting to create a build/cross-compiler environment) and I'm getting stuck at:

MAKEINFO='${SHELL} /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/build-aux/missing --run makeinfo'

Here's the log file from the 'bitbake fsl-image-gui' command:

Any suggestions would be greatly appreciated.

much thanks,

Bill

bgoetz@volta18:~/unix$ cat /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/build/config.log
This file contains any messages produced by compilers while
running configure, to aid debugging if configure makes a mistake.

It was created by GNU Autoconf configure 2.69, which was
generated by GNU Autoconf 2.69. Invocation command line was

$ ../autoconf-2.69/configure --build=x86_64-linux --host=x86_64-linux --target=x86_64-linux --prefix=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr --exec_prefix=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr --bindir=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/bin --sbindir=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/sbin --libexecdir=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/libexec --datadir=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/share --sysconfdir=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/etc --sharedstatedir=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/com --localstatedir=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/var --libdir=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/lib --includedir=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/include --oldincludedir=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/include --infodir=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/share/info --mandir=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/share/man --disable-silent-rules --disable-dependency-tracking ac_cv_path_M4=m4 ac_cv_prog_TEST_EMACS=no

## --------- ##
## Platform. ##
## --------- ##

hostname = volta18
uname -m = x86_64
uname -r = 5.0.0-31-generic
uname -s = Linux
uname -v = #33~18.04.1-Ubuntu SMP Tue Oct 1 10:20:39 UTC 2019

/usr/bin/uname -p = unknown
/bin/uname -X = unknown

/bin/arch = unknown
/usr/bin/arch -k = unknown
/usr/convex/getsysinfo = unknown
/usr/bin/hostinfo = unknown
/bin/machine = unknown
/usr/bin/oslevel = unknown
/bin/universe = unknown

PATH: /export/users/bgoetz/var-fsl-yocto/sources/poky/scripts/native-intercept
PATH: /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/bin/texinfo-dummy-native
PATH: /export/users/bgoetz/var-fsl-yocto/sources/poky/scripts
PATH: /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/bin/x86_64-linux
PATH: /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/bin
PATH: /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/sbin
PATH: /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/bin
PATH: /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/sbin
PATH: /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/bin
PATH: /export/users/bgoetz/var-fsl-yocto/sources/poky/bitbake/bin
PATH: /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/hosttools


## ----------- ##
## Core tests. ##
## ----------- ##

configure:1796: checking for a BSD-compatible install
configure:1864: result: /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/hosttools/install -c
configure:1875: checking whether build environment is sane
configure:1925: result: yes
configure:2066: checking for a thread-safe mkdir -p
configure:2105: result: /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/hosttools/mkdir -p
configure:2118: checking for gawk
configure:2134: found /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/hosttools/gawk
configure:2145: result: gawk
configure:2156: checking whether make sets $(MAKE)
configure:2178: result: yes
configure:2261: error: cannot run /bin/bash ../autoconf-2.69/build-aux/config.sub

## ---------------- ##
## Cache variables. ##
## ---------------- ##

ac_cv_env_EMACSLOADPATH_set=
ac_cv_env_EMACSLOADPATH_value=
ac_cv_env_EMACS_set=
ac_cv_env_EMACS_value=
ac_cv_env_M4_set=
ac_cv_env_M4_value=
ac_cv_env_build_alias_set=set
ac_cv_env_build_alias_value=x86_64-linux
ac_cv_env_host_alias_set=set
ac_cv_env_host_alias_value=x86_64-linux
ac_cv_env_target_alias_set=set
ac_cv_env_target_alias_value=x86_64-linux
ac_cv_path_M4=m4
ac_cv_path_PERL='/usr/bin/env perl'
ac_cv_path_install='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/hosttools/install -c'
ac_cv_path_mkdir=/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/hosttools/mkdir
ac_cv_prog_AWK=gawk
ac_cv_prog_TEST_EMACS=no
ac_cv_prog_make_make_set=yes
lt_cv_sys_lib_dlsearch_path_spec='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/lib /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/lib /lib /lib64 /usr/lib /usr/lib64'

## ----------------- ##
## Output variables. ##
## ----------------- ##

ACLOCAL='${SHELL} /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/build-aux/missing --run aclocal-1.11'
AMTAR='${SHELL} /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/build-aux/missing --run tar'
AUTOCONF='${SHELL} /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/build-aux/missing --run autoconf'
AUTOHEADER='${SHELL} /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/build-aux/missing --run autoheader'
AUTOMAKE='${SHELL} /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/build-aux/missing --run automake-1.11'
AWK='gawk'
CYGPATH_W='echo'
DEFS=''
ECHO_C=''
ECHO_N='-n'
ECHO_T=''
EGREP=''
EMACS=''
EMACSLOADPATH=''
EXPR=''
GREP=''
HELP2MAN=''
INSTALL_DATA='${INSTALL} -m 644'
INSTALL_PROGRAM='${INSTALL}'
INSTALL_SCRIPT='${INSTALL}'
INSTALL_STRIP_PROGRAM='$(install_sh) -c -s'
LIBOBJS=''
LIBS=''
LTLIBOBJS=''
M4=''
M4_DEBUGFILE=''
M4_GNU=''
MAKEINFO='${SHELL} /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/build-aux/missing --run makeinfo'
MAKE_CASE_SENSITIVE_FALSE=''
MAKE_CASE_SENSITIVE_TRUE=''
MKDIR_P='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/hosttools/mkdir -p'
PACKAGE='autoconf'
PACKAGE_BUGREPORT='[email protected]'
PACKAGE_NAME='GNU Autoconf'
PACKAGE_STRING='GNU Autoconf 2.69'
PACKAGE_TARNAME='autoconf'
PACKAGE_URL='http://www.gnu.org/software/autoconf/'
PACKAGE_VERSION='2.69'
PATH_SEPARATOR=':'
PERL=''
PERL_FLOCK=''
SED=''
SET_MAKE=''
SHELL='/bin/bash'
STRIP='strip'
TEST_EMACS=''
VERSION='2.69'
ac_cv_dir_trailing_space=''
ac_cv_sh_n_works=''
ac_cv_unsupported_fs_chars=''
am__isrc=' -I$(srcdir)'
am__leading_dot='.'
am__tar='${AMTAR} chof - "$$tardir"'
am__untar='${AMTAR} xf -'
bindir='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/bin'
build='x86_64-linux'
build_alias='x86_64-linux'
build_cpu=''
build_os=''
build_vendor=''
datadir='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/share'
datarootdir='${prefix}/share'
docdir='${datarootdir}/doc/${PACKAGE_TARNAME}'
dvidir='${docdir}'
exec_prefix='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr'
host='x86_64-linux'
host_alias='x86_64-linux'
host_cpu=''
host_os=''
host_vendor=''
htmldir='${docdir}'
includedir='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/include'
infodir='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/share/info'
install_sh='${SHELL} /export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/autoconf-2.69/build-aux/install-sh'
libdir='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/lib'
libexecdir='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/libexec'
lispdir=''
localedir='${datarootdir}/locale'
localstatedir='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/var'
mandir='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/share/man'
mkdir_p='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/hosttools/mkdir -p'
oldincludedir='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/include'
pdfdir='${docdir}'
prefix='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr'
program_transform_name='s,x,x,'
psdir='${docdir}'
sbindir='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/usr/sbin'
sharedstatedir='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/com'
sysconfdir='/export/users/bgoetz/var-fsl-yocto/build_xwayland/tmp/work/x86_64-linux/autoconf-native/2.69-r11/recipe-sysroot-native/etc'
target_alias='x86_64-linux'

## ----------- ##
## confdefs.h. ##
## ----------- ##

/* confdefs.h */
#define PACKAGE_NAME "GNU Autoconf"
#define PACKAGE_TARNAME "autoconf"
#define PACKAGE_VERSION "2.69"
#define PACKAGE_STRING "GNU Autoconf 2.69"
#define PACKAGE_BUGREPORT "[email protected]"
#define PACKAGE_URL "http://www.gnu.org/software/autoconf/"
#define PACKAGE "autoconf"
#define VERSION "2.69"

configure: exit 2
bgoetz@volta18:~/unix$

0 Kudos
Reply
2 Replies

1,775 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Bill Goetz,

It seems that you are using the Variscite yocto BSP. I would recommend not changing anything from the default setup and try baking the fsl-image-gui first jus to make sure that the default setup is working correctly. Then work on your changes. There is a lot of useful information and forums on the Yocto Project side.

Regards,

0 Kudos
Reply

1,775 Views
bgoetz
Contributor I

Hello, yes, thanks for the reply!

I’m working with the Variscite guys to get a build.

Thanks again!

Bill

0 Kudos
Reply