android no HDMI output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

android no HDMI output

1,477 Views
mm2021
Contributor III

I download android-11.0.0_2.0.0_image_8mmevk.tar.gz and burn eMMC by:

uuu_imx_android_flash.bat -f imx8mm -a -e -d mipi-panel -c 28

 

The android bootd up successfully and message comes from usb-uart, but HDMI does not have output. The monitor shows no signal. But if I download linux kernel, HDMI has output.

 

I also tried android-10.0.0_2.6.0_image_8mmevk.tar.gz, still failed at HDMI.

So anybody can give some clues?

 

0 Kudos
Reply
1 Reply

1,473 Views
Yuri
NXP Employee
NXP Employee

@mm2021 
Hello,

   Have You used recommendations of the start guide how to transfer image and configure
U-Boot environment variables for the HDMI?

https://www.nxp.com/docs/en/quick-reference-guide/ANDROID_QUICK_START_GUIDE.pdf

 

Regards,
Yuri.

0 Kudos
Reply