android_M6.0.1_2.1.0 start problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

android_M6.0.1_2.1.0 start problem

1,154 次查看
yuminmin
Contributor I

 I  building android image for the SD card on the SABRE-SD board,then start this image

init: cannot find '/system/bin/surfaceflinger', disabling 'surfaceflinger'
init: write_file: Unable to open '/sys/block/mmcblk0/queue/read_ahead_kb': No such file or directory
init: write_file: Unable to open '/sys/block/mmcblk1/queue/read_ahead_kb': No such file or directory
rfkill: BT RF going to : off
init: property_set("ro.ril.wake_lock_timeout", "300") failed
init: property 'ro.product.manufacturer' doesn't exist while expanding '${ro.product.manufacturer}'
init: cannot expand '${ro.product.manufacturer}' while writing to '/config/usb_gadget/g1/strings/0x409/manufacturer'
init: property 'ro.product.model' doesn't exist while expanding '${ro.product.model}'
init: cannot expand '${ro.product.model}' while writing to '/config/usb_gadget/g1/strings/0x409/product'
binder: 195:195 transaction failed 29189, size 0-0
binder: 195:195 transaction failed 29189, size 0-0
binder: 195:195 transaction failed 29189, size 0-0
binder: 195:195 transaction failed 29189, size 0-0

help me to solve this one thanks in advance

0 项奖励
回复
1 回复

967 次查看
jimmychan
NXP TechSupport
NXP TechSupport

according to the error message, please try to re-program the images to the SD card again.

0 项奖励
回复