about uuu document

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

about uuu document

3,386件の閲覧回数
HEXER
Contributor III

Greetings community.

Am i the only one who thinks UUU pdf file's content has lots of grammatically incorrect sentences?

I don't want to be ungraceful. I am asking because i am also a non-native English speaker and i want to see correct sentences to improve/educate myself.

 

Best regards...

タグ(1)
0 件の賞賛
返信
5 返答(返信)

3,351件の閲覧回数
HEXER
Contributor III

I was referring to https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/imx-processors/140261/1/UUU.pdf

for example:

UUU design as common library and UI. So user can easily integrate into their tools with uuu library. UUU also easy run in any
scripts.

and

bootloader means bootable image, which included ROM required header. for imx6/7, it should be uboot.imx
generally. for imx8qxp\imx8qm\imx8mm\im8mq, it is flash.bin.

i find the sentences quite weird.

0 件の賞賛
返信

3,321件の閲覧回数
Mestkim
Contributor III

兄弟这个不是汉语拼音

0 件の賞賛
返信

3,333件の閲覧回数
Mestkim
Contributor III

I read the words, it is very clear. 

And I also put the words into to word to check. Here is result. It seems no grammar issue there.

 

2023-08-04_110603.png

 

 

 

 

 

0 件の賞賛
返信

3,293件の閲覧回数
HEXER
Contributor III

It seems that the issue is my bad english.

0 件の賞賛
返信

3,370件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @HEXER !

Could you please point to me what uuu.pdf are you referring?

And if you can point which sentences are incorrect.

 

Best regards.

0 件の賞賛
返信