about the CCM_ANALOG_PLL_ARM[POWERDOWN] bit for i.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

about the CCM_ANALOG_PLL_ARM[POWERDOWN] bit for i.MX6

跳至解决方案
971 次查看
yuuki
Senior Contributor II

Dear all,

Would you tell me the details of CCM_ANALOG_PLL_ARM[POWERDOWN] bit?

The CCM_ANALOG_PLL_ARM[POWERDOWN] bit reset value is "1" by default.
However, the details are not listed in description.

For example
If this bit is set to "1", PLL is powered off when i.MX6 is entered to Low power mode.
If this bit is set to "0", PLL is always powered on (regardless of Low Power mode).

May I have advice?

Best Regards,
Yuuki

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
831 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Your understanding is correct.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
832 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Your understanding is correct.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复