about the CCM_ANALOG_PLL_ARM[POWERDOWN] bit for i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about the CCM_ANALOG_PLL_ARM[POWERDOWN] bit for i.MX6

Jump to solution
873 Views
yuuki
Senior Contributor II

Dear all,

Would you tell me the details of CCM_ANALOG_PLL_ARM[POWERDOWN] bit?

The CCM_ANALOG_PLL_ARM[POWERDOWN] bit reset value is "1" by default.
However, the details are not listed in description.

For example
If this bit is set to "1", PLL is powered off when i.MX6 is entered to Low power mode.
If this bit is set to "0", PLL is always powered on (regardless of Low Power mode).

May I have advice?

Best Regards,
Yuuki

Labels (1)
0 Kudos
Reply
1 Solution
733 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Your understanding is correct.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
734 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Your understanding is correct.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply