about imx6ul_tsc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about imx6ul_tsc

1,405 Views
story
Contributor II

My chip is imx6ul, using the resistive screen, connected to the Touch Screen Controller, using 4 lines, bsp is 4.1.15.

I hold down a point, the value read during a period of time has a large deviation.
Can I improve this performance by modifying the driver and reduce the fluctuation of the value?

Labels (1)
0 Kudos
Reply
1 Reply

1,291 Views
igorpadykov
NXP Employee
NXP Employee

Hi 扬 杨 

one can try ts_calibrate

Touchscreen Test Apps 

Problems calibrating capacitive touchscreen 

touch screen Archives - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply