about XTALI Oscillator

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about XTALI Oscillator

1,559 Views
goto11
Contributor III

Hello,Community

When the power is turned on without writing software, is the 24MHz (XTALI Oscillator) of the external input clock oscillating?

best regards

Goto

Labels (1)
0 Kudos
Reply
1 Reply

1,493 Views
igorpadykov
NXP Employee
NXP Employee

Hi Goto

yes it is oscillating.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply