Yocto library link error(real-ld): cannot find /lib/libc.so.6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto library link error(real-ld): cannot find /lib/libc.so.6

ソリューションへジャンプ
23,364件の閲覧回数
Hirotoshi_Sato
Contributor II

Hi, 

I try to compile a C program using pcap with Eclipse and Yocto ADT.

After building, I got errors as bottom (config.log).

  • There are several errors.
  1. arm-fslc-linux-gnueabi-gcc: error: unrecognized command line option '-V'
  2. arm-fslc-linux-gnueabi-gcc: error: unrecognized command line option '-qversion'; did you mean '--version'?
  3. /opt/fslc-framebuffer/2.2.1/sysroots/x86_64-fslcsdk-linux/usr/libexec/arm-fslc-linux-gnueabi/gcc/arm-fslc-linux-gnueabi/6.2.0/real-ld: cannot find /lib/libc.so.6
    /opt/fslc-framebuffer/2.2.1/sysroots/x86_64-fslcsdk-linux/usr/libexec/arm-fslc-linux-gnueabi/gcc/arm-fslc-linux-gnueabi/6.2.0/real-ld: cannot find /usr/lib/libc_nonshared.a
    /opt/fslc-framebuffer/2.2.1/sysroots/x86_64-fslcsdk-linux/usr/libexec/arm-fslc-linux-gnueabi/gcc/arm-fslc-linux-gnueabi/6.2.0/real-ld: cannot find /lib/ld-linux-armhf.so.3
    collect2: error: ld returned 1 exit status

I think the error 1 and 2 can be ignored (If there are solutions, please teach me).

However the error 3 says it cannot link library and C compiler cannot create executables.

How can I solve this error?

My environment:

Eclipse settings:

  • Properties>Autotools>Configure settings>configure>Command:
    CFLAGS=" -g -O0  -I/home/user/var-fslc-yocto/build_fb/tmp/sysroots/imx6ul-var-dart/usr/include --sysroot=/opt/fslc-framebuffer/2.2.1/sysroots/armv7at2hf-neon-fslc-linux-gnueabi" CXXFLAGS=" -g -O0  --sysroot=/opt/fslc-framebuffer/2.2.1/sysroots/armv7at2hf-neon-fslc-linux-gnueabi" LDFLAGS=" -L/opt/fslc-framebuffer/2.2.1/sysroots/armv7at2hf-neon-fslc-linux-gnueabi -L/home/user/var-fslc-yocto/build_fb/tmp/sysroots/imx6ul-var-dart -L/home/user/var-fslc-yocto/build_fb/tmp/sysroots/imx6ul-var-dart/usr/lib  --sysroot=/opt/fslc-framebuffer/2.2.1/sysroots/armv7at2hf-neon-fslc-linux-gnueabi" CPPFLAGS=" --sysroot=/opt/fslc-framebuffer/2.2.1/sysroots/armv7at2hf-neon-fslc-linux-gnueabi" configure --with-libtool-sysroot=/opt/fslc-framebuffer/2.2.1/sysroots/armv7at2hf-neon-fslc-linux-gnueabi 
  • All options:
     --host=arm-fslc-linux-gnueabi --build=x86_64-linux --target=arm-fslc-linux-gnueabi  

What I checked

  • under sysroots (=/opt/fslc-framebuffer/2.2.1/sysroots/armv7at2hf-neon-fslc-linux-gnueabi ), there are lib/libc.so.6, usr/lib/libc_nonshared.a, lib/ld-linux-armhf.so.3. However config.log says cannot find them.
  • https://community.nxp.com/thread/322870  this link treat the same problem, but I cannot understan what I should do (I think I may set the same settings as this link.).

config.log

configure:3187: arm-fslc-linux-gnueabi-gcc -march=armv7-a -mthumb -mfpu=neon -mfloat-abi=hard --sysroot=/opt/fslc-framebuffer/2.2.1/sysroots/armv7at2hf-neon-fslc-linux-gnueabi -V >&5
arm-fslc-linux-gnueabi-gcc: error: unrecognized command line option '-V'
arm-fslc-linux-gnueabi-gcc: fatal error: no input files
compilation terminated.
configure:3198: $? = 1
configure:3187: arm-fslc-linux-gnueabi-gcc -march=armv7-a -mthumb -mfpu=neon -mfloat-abi=hard --sysroot=/opt/fslc-framebuffer/2.2.1/sysroots/armv7at2hf-neon-fslc-linux-gnueabi -qversion >&5
arm-fslc-linux-gnueabi-gcc: error: unrecognized command line option '-qversion'; did you mean '--version'?
arm-fslc-linux-gnueabi-gcc: fatal error: no input files
compilation terminated.
configure:3198: $? = 1
configure:3218: checking whether the C compiler works
configure:3240: arm-fslc-linux-gnueabi-gcc -march=armv7-a -mthumb -mfpu=neon -mfloat-abi=hard --sysroot=/opt/fslc-framebuffer/2.2.1/sysroots/armv7at2hf-neon-fslc-linux-gnueabi -g -O0 -I/home/user/var-fslc-yocto/build_fb/tmp/sysroots/imx6ul-var-dart/usr/include --sysroot=/opt/fslc-framebuffer/2.2.1/sysroots/armv7at2hf-neon-fslc-linux-gnueabi --sysroot=/opt/fslc-framebuffer/2.2.1/sysroots/armv7at2hf-neon-fslc-linux-gnueabi -L/opt/fslc-framebuffer/2.2.1/sysroots/armv7at2hf-neon-fslc-linux-gnueabi -L/home/user/var-fslc-yocto/build_fb/tmp/sysroots/imx6ul-var-dart -L/home/user/var-fslc-yocto/build_fb/tmp/sysroots/imx6ul-var-dart/usr/lib --sysroot=/opt/fslc-framebuffer/2.2.1/sysroots/armv7at2hf-neon-fslc-linux-gnueabi conftest.c >&5
/opt/fslc-framebuffer/2.2.1/sysroots/x86_64-fslcsdk-linux/usr/libexec/arm-fslc-linux-gnueabi/gcc/arm-fslc-linux-gnueabi/6.2.0/real-ld: cannot find /lib/libc.so.6
/opt/fslc-framebuffer/2.2.1/sysroots/x86_64-fslcsdk-linux/usr/libexec/arm-fslc-linux-gnueabi/gcc/arm-fslc-linux-gnueabi/6.2.0/real-ld: cannot find /usr/lib/libc_nonshared.a
/opt/fslc-framebuffer/2.2.1/sysroots/x86_64-fslcsdk-linux/usr/libexec/arm-fslc-linux-gnueabi/gcc/arm-fslc-linux-gnueabi/6.2.0/real-ld: cannot find /lib/ld-linux-armhf.so.3
collect2: error: ld returned 1 exit status
configure:3244: $? = 1
configure:3282: result: no
configure: failed program was:
| /* confdefs.h */
| #define PACKAGE_NAME "packetcapture"
| #define PACKAGE_TARNAME "packetcapture"
| #define PACKAGE_VERSION "0.1.0"
| #define PACKAGE_STRING "packetcapture 0.1.0"
| #define PACKAGE_BUGREPORT ""
| #define PACKAGE_URL ""
| #define PACKAGE "packetcapture"
| #define VERSION "0.1.0"
| /* end confdefs.h. */
|
| int
| main ()
| {
|
| ;
| return 0;
| }
configure:3287: error: in `/home/user/workspace/packetcapture':
configure:3289: error: C compiler cannot create executables
See `config.log' for more details

ラベル(4)
0 件の賞賛
返信
1 解決策
18,604件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Hirotoshi Sato,

Are you still experiencing this error? I’m no familiar with the Variscite toolchain and BSP but it looks like the problem is that the path to the libraries is not correct. Perhaps it’s looking for the libraries on the path of the host and not the sysroot of the BSP.

Have you set the flags as shown on the following Yocto document?

https://www.yoctoproject.org/docs/1.6/adt-manual/adt-manual.html#makefile-based-projects

I hope this helps!

Regards,

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
18,605件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Hirotoshi Sato,

Are you still experiencing this error? I’m no familiar with the Variscite toolchain and BSP but it looks like the problem is that the path to the libraries is not correct. Perhaps it’s looking for the libraries on the path of the host and not the sysroot of the BSP.

Have you set the flags as shown on the following Yocto document?

https://www.yoctoproject.org/docs/1.6/adt-manual/adt-manual.html#makefile-based-projects

I hope this helps!

Regards,

0 件の賞賛
返信
18,604件の閲覧回数
Hirotoshi_Sato
Contributor II

I am sorry late notice... 

As you mentioned, I had to modify library path.

Thank you!

0 件の賞賛
返信