Yocto imx-linux-sumo can't boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto imx-linux-sumo can't boot

2,401件の閲覧回数
erikraynolds
Contributor IV

After building an image out of 

repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-sumo -m imx-4.14.78-1.0.0_ga.xml

build on 8qm machine

MACHINE=imx8qmmek DISTRO=fsl-imx-xwayland source ./fsl-setup-release.sh -b bld-xwayland

the image can't boot ...

sudo dd if=core-image-minimal-imx8qmmek.sdcard of=/dev/mmcblk0 bs=1M conv=fsync

タグ(2)
0 件の賞賛
返信
5 返答(返信)

1,958件の閲覧回数
s233199
Contributor II

Hi, I have the same problem, I am building for an imx8qmlpddr4amr2 machine, using imx-4.14.78-1.0.0_ga.xml. I can build but the image can't boot. Have you find a solution?

0 件の賞賛
返信

1,958件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

which image doesn't work? the image you build with xwayland or core-image-minimal-imx8qmmek.sdcard?

0 件の賞賛
返信

1,958件の閲覧回数
erikraynolds
Contributor IV

core-image-minimal

0 件の賞賛
返信

1,958件の閲覧回数
erikraynolds
Contributor IV

I can build core-image-minimal 

bitbake core-image-minimal

There is no problem to build but after flashing on sdcard that sdcard image (core-image-minimal) is not booting ...

I showed all procedure I am doing above.

0 件の賞賛
返信

1,958件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

could you boot up with demo image? any log file with this?

0 件の賞賛
返信