Yocto & gst-plugins-bad help

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto & gst-plugins-bad help

3,767件の閲覧回数
timothybean
Contributor IV

Can someone please help with installing gst-plugins-bad in Yocto? I include "gst-plugins-bad-mpegtsdemux" to be installed bu I get an error:

DEBUG: Executing shell function do_rootfs

| Note: configuring RPM platform settings

| Note: configuring RPM system provides

| Note: configuring RPM DB settings

| Note: configuring Smart settings

|

|

|

|

|

|

| Note: adding Smart channel nitrogen6x (80)

|

|

| Note: adding Smart channel armv7a_vfp_neon (75)

|

|

| Note: adding Smart channel all (10)

|

|

| Note: configuring RPM cross-install scriptlet_wrapper

|

| Updating cache...               ######################################## [100%]

|

| Saving cache...

|

| Note: adding Smart RPM DB channel

|

| Note: to be installed:  libsoup-2.4@armv7a_vfp_neon firmware-imx-vpu-imx6q@nitrogen6x libgtop-2.0-7@armv7a_vfp_neon rpm-postinsts@all packagegroup-core-nfs-server@all python-subprocess@armv7a_vfp_neon vbmediaserver@armv7a_vfp_neon gst-plugins-base-tcp@nitrogen6x packagegroup-fsl-gstreamer@nitrogen6x python-datetime@armv7a_vfp_neon python-json@armv7a_vfp_neon packagegroup-core-boot@nitrogen6x

| Loading cache...

| Updating cache...               ######################################## [100%]

|

| Computing transaction...error: Can't install libglib-2.0-utils-1:2.34.3-r2@armv7a_vfp_neon: no package provides /usr/local/bin/python

|

| Saving cache...

|

| ERROR: Function failed: do_rootfs (see /home/tim/imx/yocto/fsl-community-bsp/build/tmp/work/nitrogen6x-poky-linux-gnueabi/n6x-min/1.0-r0/temp/log.do_rootfs.18452 for further information)

ERROR: Task 7 (/home/tim/imx/yocto/fsl-community-bsp/sources/meta-n6x-min/recipes-fsl/images/n6x-min.bb, do_rootfs) failed with exit code '1'

Thanks for any help.

Tim

ラベル(5)
0 件の賞賛
返信
4 返答(返信)

3,140件の閲覧回数
LeonardoSandova
Specialist I

Can you share your local.conf file? Did you start baking from a empty tmp file?

0 件の賞賛
返信

3,140件の閲覧回数
timothybean
Contributor IV

Tried baking from both empty and already built images. Here is local.conf:

LCONF_VERSION = "6"

BBPATH = "${TOPDIR}"

BSPDIR := "${@os.path.abspath(os.path.

dirname(d.getVar('FILE', True)) + '/../..')}"

BBFILES ?= ""
BBLAYERS = " \
  ${BSPDIR}/sources/poky/meta \
  ${BSPDIR}/sources/poky/meta-yocto \
   \
  ${BSPDIR}/sources/meta-openembedded/meta-oe \
  \
  ${BSPDIR}/sources/meta-fsl-arm \
  ${BSPDIR}/sources/meta-fsl-arm-extra \
  ${BSPDIR}/sources/meta-n6x-min \
"

meta-n6x-min is a image recipe I made. (copy of image-test)

Thanks

Tim

0 件の賞賛
返信

3,140件の閲覧回数
timothybean
Contributor IV

Anyone have an idea?

0 件の賞賛
返信

3,140件の閲覧回数
LeonardoSandova
Specialist I

seems that you posted the bblayers.conf and not the local.conf.

0 件の賞賛
返信