We want to create a Yocto build for iMX8M Plus. We are following the instructions as mentioned in the following user guide.
https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf
The issue is we are confused as to which machine name do we need to use:
1. imx8mp-lpddr4-evk
2. imx8mp-ddr4-evk
For the moment we have used imx8mp-lpddr4-evk. For the distro we have used fsl-imx-xwayland. Once the build is done, we have used a 16 GB SD Card and flashed the wic using the following command:
zstdcat .wic.zst | sudo dd of=/dev/sd bs=1M conv=fsync
But when using the SD Card, the boot does not happen, and we are not able to see any logs in the minicom (it is connected to the debug port to the PC). We tried using /dev/ttyUSB0 but did not see any logs.
So please do let us know which machine name to use (1) or (2). What mistake are we making for which Yocto is not running on the iMX8m plus board
已解决! 转到解答。
Hi @soumyakk!
Let me provide the steps I have followed and tested on my side that should work.
Format SD card connected to my Linux PC, listed as sdb
$ sudo fdisk /dev/sdb
Type the following parameters (each followed by
p [lists the current partitions]
d [to delete existing partitions. Repeat this until no unnecessary partitions are reported by the 'p' command to start fresh.]
n [create a new partition]
p [create a primary partition - use for both partitions]
1 [the first partition]
20480 [starting at offset sector]
1024000 [ending position of the first partition to be used for the boot images]
p [to check the partitions]
n
p
2
1228800 [starting at offset sector, which leaves enough space for the kernel, the bootloader and its configuration data]
<enter> [using the default value will create a partition that extends to the last sector of the media]
p [to check the partitions]
w [this writes the partition table to the media and fdisk exits]
Change directory to where I have all my files, ubot, rootfs, dtb, etc.
$ cd LF_v5.15.32-2.0.0_images_imx8mnevk/
Copy bootloader to SD card
$ sudo dd if=imx-boot-imx8mnevk-sd.bin-flash_evk of=/dev/sdb bs=1k seek=32 conv=fsync
Create a VFAT partition where kernel and dtb will be stored
$ sudo mkfs.vfat /dev/sdb1
Create a directory where SD partition will be mounted; next mount the partition
$ mkdir mountpoint
$ sudo mount /dev/sdb1 mountpoint
Copy and rename kernel image and dtb (here the documentation is not clear, so this may be the cause of your issue) uboot expects that kernel image is named Image and dtb imx8mq-evk.dtb
$ sudo cp Image-imx8mnevk.bin ./mountpoint/Image
$ sudo cp imx8mq-evk.dtb ./mountpoint/imx8mq-evk.dtb
Unmount the partition
$ sudo umount mountpoint
Format partition that will store the root file system
$ sudo mkfs.ext4 /dev/sdb2
Mount the partiotion
$ sudo mount /dev/sdb2 mountpoint/
Create a directory and extract root file system
$ mkdir rootfs
$ cd rootfs/
$ tar -jxvf ../imx-image-full-imx8mnevk.tar.bz2
Copy root file system to the mounted partition
$ sudo cp -a * ../mountpoint
Unmount partition and sync
$ sudo umount ../mountpoint
$ sync
You may unplug your SD card now and try it on your board, if you find any issue please do let me know.
https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf
Best Regards!
Chavira
i followed you flashing guidelines for imx8mplus evk , it is working.
On what basis we select partition1 first sector and end sector , second partition first sector and end sector . where this information present .please help me out.
Thanks&Regards
Hi @soumyakk !
Both are for imx8mp, the difference is the RAM (one uses lpddr4 and the other uses ddr4).
If you are not sure what board are you using, put the machine on "imx8mpevk" to generate both bootloaders.
https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf
Best Regards!
Chavira