Yocto U-Boot SPL not loading

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto U-Boot SPL not loading

3,430件の閲覧回数
maxime_borges
Contributor I

Hello,

I'm building a Poky distribution for an OPOS6ULdev, and I can't get my U-Boot (FSLC) SPL binary to boot.

Armadeus is giving U-Boot image and SPL for version 2018.05, but my distribution is building the version 2018.07 and I'd like to use it.

I'm able to boot the distribution using the U-Boot image and rootfs from my Yocto build, but I have to use the SPL from Armadeus, otherwise the board simply doesn't boot.

I have the buildroot project that built the 2018.05 working version and there is no specific patch for this version since this board is supported by mainline U-Boot.

I'm using a script based on the u-boot recovery script from Armadeus to automate my workflow, but using exactly the script linked and replacing with my SPL doesn't help.

The first part of this script using imx_usb works, and I can see it boot my SPL at this stage, download and flash the U-Boot image and SPL using CLI. But after that when I reset my board nothing is happening.

When I use the exact same script but using the SPL from Armadeus, I can boot the board.

I tried to enable every logging I could when building the SPL but nothing is happening again.

I joined the two SPL binaries and the Yocto machine configuration I'm using.

Any clue on what's wrong ?

ラベル(2)
1 返信

2,858件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Maxime

nxp do not use spl for its i.MX6 uboot releases, in general also this may be posted on

meta-fsl-arm mailing list
meta-freescale Info Page 

below is tutorial how use spl

http://trac.gateworks.com/wiki/ventana/bootloader 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------