Yocto MIPI driver for iMX8M Mini

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Yocto MIPI driver for iMX8M Mini

4,824 次查看
Alirezah95
Contributor II

Hi,

I'm working on a Yocto image for iMX8M Mini and I've created an image for imx8mm-lpddr4-evk machine on the kirkstone branch. The problem is that is looks like mipi driver is not included in the image and therefore nothing is displayed when the board is connected to an hdmi display using mipi-hdmi converter. I've also enabled mipi module for iMX.7 and iMX.8 from the bitbake menuconfig but it did not work too. How can i correctly add the required modules?

0 项奖励
回复
4 回复数

4,783 次查看
Alirezah95
Contributor II

@Zhiming_Liu  It looks like kirsktone branch of meta-freescale has issues. I switched to dunfell and display is working fine.  I've compared .config files of both branches and it turns out that in kirkstone no option about MIPI is enabled in the config file, while in dunfell we have all these modules enabled. 

Part of uboot logs in dunfell image:

[*]-Video Link 0 (1920 x 1080)
        [0] lcdif@32e00000, video
        [1] mipi_dsi@32e10000, video_bridge
        [2] adv7535@3d, panel

0 项奖励
回复

4,710 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @Alirezah95 

The demo images are compiled from same Yocto project, there should not have issues if demo images can work.

0 项奖励
回复

4,796 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Have you tried demo images on website?

0 项奖励
回复

4,789 次查看
Alirezah95
Contributor II

Yes and they all work fine.

0 项奖励
回复