Yocto Linux on IMX6slevk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Yocto Linux on IMX6slevk

10,029 Views
sandeepajesh
Contributor III

Hi NXP

We have purchased a new imx6sl Evsal board. Below one:-

i.MX 6SoloLite Evaluation Kit|NXP 

I need to put Yocto Linux on it. Can you please help me with the steps.

Regards

Sandeep S

Labels (1)
Tags (1)
4 Replies

9,896 Views
jan_spurek
NXP Employee
NXP Employee

Hi,

you can find the software here: http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Just download desired BSP, extract the image and load it into an SD card.

Regards,

Jan

0 Kudos
Reply

9,896 Views
sandeepajesh
Contributor III

I think its for Android. But as per our requirement we need to put poky-linux on it.

Can you please help in getting yocto material.

Thx-

Sandeep S

0 Kudos
Reply

9,894 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sandeep

seems most simple is to use mfgtool2-yocto-mx-evk-sdcard-sd2.vbs
script with default images included in MFG Tools. Use attached Linux Guide,
sect.4.5.2 Booting from an SD card in slot SD2, included in Doc package
http://www.nxp.com/webapp/Download?colCode=L4.1.15_1.1.0_LINUX_DOCS&Parent_nodeId=133769948107170617...

Programmers (Flash, etc.) (14)
IMX6_L4.1.15_1.1.0_MFG_TOOL (REV L4.1.15_1.1.0)
http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards
igor

9,894 Views
jan_spurek
NXP Employee
NXP Employee

That is because you are probably looking only to "Recommended Software & tools" section. You need to scroll down to "Board support packages" and then click the "more" button. Then you will find also Linux BSPs.

Regards,
Jan

0 Kudos
Reply