Xen with Android

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Xen with Android

1,202 Views
wang12zhe
Contributor III

I‘m compile android_automotive-10.0.0_1.1.0source code follow Android_User's_Guide.pdf

step1 : source build/envsetup.sh 

step2 : lunch mek_8q_car2-userdebug

step3: ./imx-make.sh bootloader -j4 

step4:  ./imx-make.sh kernel -j4 

step5:  ./imx-make.sh -j4 

when I try to run "sudo ./uuu_imx_android_flash.sh -f imx8qm -d xen" will show error as below:

This script is validated with uuu 1.3.124 version, it is recommended to align with this version.
dual bootloader is supported
dtbo is supported
dual slot is supported
generate lines to flash partition-table.img to the partition of gpt
generate lines to flash bootloader-imx8qm-xen.img to the partition of bootloader_a
generate lines to flash dtbo-imx8qm-xen.img to the partition of dtbo_a
generate lines to flash boot.img to the partition of boot_a
generate lines to flash system.img to the partition of system_a
generate lines to flash vendor.img to the partition of vendor_a
generate lines to flash product.img to the partition of product_a
generate lines to flash vbmeta-imx8qm-xen.img to the partition of vbmeta_a
generate lines to flash bootloader-imx8qm-xen.img to the partition of bootloader_b
generate lines to flash dtbo-imx8qm-xen.img to the partition of dtbo_b
generate lines to flash boot.img to the partition of boot_b
generate lines to flash system.img to the partition of system_b
generate lines to flash vendor.img to the partition of vendor_b
generate lines to flash product.img to the partition of product_b
generate lines to flash vbmeta-imx8qm-xen.img to the partition of vbmeta_b
uuu script generated, start to invoke uuu with the generated uuu script
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.139-0-g1a8f760

Wait for Known USB Device Appear...
Error: fail open file: >/tmp/bootloader-imx8qm-xen.img

then checked :

owenn@kostalaen-HP-ProDesk-600-G3-MT:~/8TB/AndroidProject/Android10/android_build$ ls /tmp/bootloader-imx8qm-xen.img -l
lrwxrwxrwx 1 root root 111 12月 25 08:39 /tmp/bootloader-imx8qm-xen.img -> /home/owenn/8TB/AndroidProject/Android10/android_build/out/target/product/mek_8q/bootloader-imx8qm-xen.img

but I can't find bootloader-imx8qm-xen.img in out/target/product/mek_8q/ 

anyone can help me and give suggestion? thank very much

0 Kudos
Reply
0 Replies