XEN on i.MX8QXP MEK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

XEN on i.MX8QXP MEK

2,720 Views
stevejang
Contributor I

Dears,

I want to test the virtualization with Xen on i.mx8qxp mek board.

I built yocto image with xen and have tried to find the configuration for domU.

Then kernel doesn't have domU dtb for imx8qxp while has for imx8qm, fsl-imx8qm-mek-dom0.dtb.

Furthermore I can't find domU configuration for imx8qxp as domu-imx8qm-mek.cfg.

Is there a person that already test XEN on i.MX8QXP board?

Please help me set it up correctly.

0 Kudos
Reply
4 Replies

2,473 Views
Peng_Fan
NXP Employee
NXP Employee

What usecase are u you tring to use XEN on i.MX8QXP MEK? xen on i.MX8QXP is only basic feature because there is no SMMU in this chip.

Kernel & Virtualization Engineer
0 Kudos
Reply

2,449 Views
jpknuuti
Contributor I

Does i.MX8X has Xen support?

0 Kudos
Reply

2,473 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello,

We are in a pre-release state, so we do not have officially support for XEN or JAILHOUSE at this moment, it is in a BETA phase.  I apologize for this inconvenience.

- Virtualization L_VIRT_4.14.78_1.0.0_4.11_0.9.1_beta - Jailhouse Demo

0 Kudos
Reply

2,322 Views
shaoxiao_guo_dn
Contributor I

Does imx8qxp mek support XEN now?

0 Kudos
Reply