XEN cpu0 panic

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

XEN cpu0 panic

1,402件の閲覧回数
Ahelion
Contributor IV

Hello all,

I have a linux downloaded from nxp imx8qm mek LF6 variant, I generated a XEN binary using the yocto for said variant, copied the XEN binary to boot, also copied the imx8qm-mek-dom0.dtb from linux 5.10 to boot. after reset in u-boot I gave this command: run xenmmcboot, and got this ( see attachment )

Screenshot from 2024-03-20 13-23-46.png

any ideea how to fix it?

 

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,379件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

 

Make sure that the XEN boot is for the device you are trying to boot, looks like is for MX8QX that not correspond to MX8QM.

Regards

0 件の賞賛
返信

1,368件の閲覧回数
Ahelion
Contributor IV
from the imx8qm yocto i generated the Xen binary, and the dts I took from the linux 5.10 zip file from the same imx8qm mek page.
0 件の賞賛
返信