X11 Forwarding not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

X11 Forwarding not working

2,810件の閲覧回数
guna007
Contributor III

I recently upgraded from jethro branch to morty branch. After that, X11 forwarding is not working?

Notes:

Kernel: 4.1.x

Image: core-image-multimedia-full

Configuration: X11Forwarding is enabled in /etc/ssh/sshd_config file in the board.

ラベル(5)
タグ(3)
3 返答(返信)

2,536件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello OtavioSalvador ‌, would you know if there is a known issue regarding this on the Morty branch?

Regards,

0 件の賞賛
返信

2,536件の閲覧回数
OtavioSalvador
Senior Contributor II

Hello gusarambula‌, I did fix this in past for a customer. If I recall correctly, the cause of the change was a more strict default setting from OpenSSH and I ended adjusting it for the customer's needs.

2,536件の閲覧回数
guna007
Contributor III

I found xauth is missing in the image . When I added that to image, it's working now!