Hi,
We are working on iMX8MQ based custom board. We have calculated the internal worst-case power consumption on iMX8MQ processor using NXP iMX8MQ EVK board as a reference. We understand that the typical power consumption depends on the use case.
The EVK power consumption value derived from the above calculation is too high (~14.8W).
We found one application note, AN12118, which shows the power consumption of iMX8M processor is <4W.
So we want to understand, why the EVK power distribution is designed for such high power, ~14.8W?
We do not want to over budget our power supply design for iMX8MQ processor.
Thanks.
The worst case power consumption umbers can be calculated from the maximum supply current numbers for various power rails, given in the Table 9 of the i.MX8M Data Sheet document, available on the processor's Documentation web page:
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I assume you used the maximum values of Table 9 in the 8M Data Sheet for this calculation.
This a very very pessimistic approach for an overall maximum power consumption.
Let me provide some explanations:
Regards,
Bernhard.
Thank you very much Bernhard.
This is indeed a very helpful information.
Appreciate your inputs.
Thanks.