Windows 8 on ARM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Windows 8 on ARM

2,524件の閲覧回数
seetha
Contributor III

Hi all,

Does anybody know about Windows 8 BSP on ARM availability. If so please let me know the site from where I can download it or buy it.

And also please let me know if any demo image for ARM available.

Thanks

With Regards,

Seetharam

ラベル(1)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,997件の閲覧回数
iMXAndrew
Contributor II

Seetharam,

 

WOA is going to be called Windows RT, as of right now. Don't ask me why Microsoft decided to call it that, but that is what I have been told 2 days ago. It will be released the 3rd or 4th quarter 2012. I have asked Freescale about if they are going to support this platform. Freescale has not answering this question yet, but us developers would like to know this information as this gives us an idea on the hardware we need to get for development.

 

I would imagine that if they did support it, it would be for the i.MX6 platforms. As one of the prefered specs for use are dual processors. I also would like a definitive answer from Freescale about this also.  

0 件の賞賛
返信

1,997件の閲覧回数
MarcCoussement
Contributor I

Any news on windows RT for I.MX6?

0 件の賞賛
返信