WiFi / wlan on core-image-full-cmdline-imx8mqevk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

WiFi / wlan on core-image-full-cmdline-imx8mqevk

1,799件の閲覧回数
purnank
Contributor I

I am trying to get WiFi up and running on iMX8, but unfortunately i am not able to get Interface wlan0 listed on the board.

Through various threads,  I have tried to wpa-supplicant,iw, etc. wireless pacakges but all steps have gone to vein. 

Any suggestion which steps I am missing to get WiFi enabled on core-image-full-cmdline-imx8mqevk ?

Here is my conf/local.conf

MACHINE ??= 'imx8mqevk'
DISTRO ?= 'fsl-imx-xwayland'
PACKAGE_CLASSES ?= "package_rpm"
EXTRA_IMAGE_FEATURES ?= "debug-tweaks"
USER_CLASSES ?= "buildstats image-mklibs image-prelink"
PATCHRESOLVE = "noop"

BB_DISKMON_DIRS ??= "\
 STOPTASKS,${TMPDIR},1G,100K \
 STOPTASKS,${DL_DIR},1G,100K \
 STOPTASKS,${SSTATE_DIR},1G,100K \
 STOPTASKS,/tmp,100M,100K \
 ABORT,${TMPDIR},100M,1K \
 ABORT,${DL_DIR},100M,1K \
 ABORT,${SSTATE_DIR},100M,1K \
 ABORT,/tmp,10M,1K"
PACKAGECONFIG_append_pn-qemu-native = " sdl"
PACKAGECONFIG_append_pn-nativesdk-qemu = " sdl"
CONF_VERSION = "1"

# UBOOT_CONFIG = "emmc"

DL_DIR ?= "${BSPDIR}/downloads/"
ACCEPT_FSL_EULA = "1"

# gmmmkkk
IMAGE_ROOTFS_EXTRA_SPACE = "4000000"

IMAGE_INSTALL_append += " cmake curl git subversion python-pip python-click python-cryptography python-pycparser python-cffi"

IMAGE_INSTALL_append += " connman connman-client"
IMAGE_INSTALL_append += " wpa-supplicant iw"

CORE_IMAGE_EXTRA_INSTALL += " packagegroup-base-wifi"

IMAGE_INSTALL_append += " linux-firmware-ath9k"

IMAGE_INSTALL_append = " \
kernel-modules \
kernel-module-qualcomm \
udev-extraconf \
wireless-tools \
wpa-supplicant \
"

INHERIT+="toaster buildhistory"

タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,280件の閲覧回数
MichaelBMiner
Contributor IV

Has a solution to this been found?

0 件の賞賛
返信

1,305件の閲覧回数
josephzhou1
Contributor V

ok

Best Regards,
Joseph Zhou Jianhui / Senior Embedded Software Engineer, Singapore
0 件の賞賛
返信

1,536件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Purnak

one can try guidelines provided in sect.4.13.7 Configuring WLAN from User Space

attached Linux Manual with Demo Umages from

i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信