Hello, Experts and friends!
Now, I want to transform a yuv video to mp4.
I run the mxc_vpu_test.out in the i.MX53 platform.
(mxc_vpu_test.out is a example program int the i.MX53 development board)
the command line as follow:
./mxc_vpu_test.out -E "-i test.yuv -o testvpu.mp4 -w 720 -h 576 -f 2 -g 25"
the format of the input file "test.yuv" as follow:
Sampling Format: yuv422 planar progressive
Componet Order: Y,U,V
Progressive,Planar
PAL 720*576
After encording finished, I got the video file "testvpu.mp4".
I play it int microsoft media player in my PC. But I find the picture's color of testvpu.mp4
is more yellow than test.yuv. It's so obvious that I don't satisfied the result.
there are the two files in attachments. you can play them and view the effect.
if ther are some parameter is error or the "mxc_vpu_test.out" need some other parameters?
How can I get a more clearly video? Thanks for any help.
Original Attachment has been moved to: testvideo.rar.zip