Why mfg tool stops loading u-boot for custom board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why mfg tool stops loading u-boot for custom board

2,084件の閲覧回数
kishoresamy26
Contributor I

I was able to flash the uboot-usb.imx file using mfgtool for the first time and during the firmware flashing process unexpectedly power is disconnected from the board.

second time uboot-usb.imx file is not loaded using mfgtool, it is getting stuck at loading file. find the log below. how to recover my board to reflash?

 

DLL version: 2.3.2
Tuesday, May 16, 2023 14:50:25 Start new logging
ModuleID[2] LevelID[10]: CMyExceptionHandler thread is running
ModuleID[2] LevelID[1]: new MxHidDeviceClass
ModuleID[2] LevelID[10]: new MxHidDevice[055257C8]
ModuleID[2] LevelID[10]: Device Manager thread is running
ModuleID[2] LevelID[10]: CmdOperation[0] device chagned and reset to state 0
ModuleID[2] LevelID[10]: ExecuteCommand--Boot[WndIndex:0], File is f1-mfgtool\Profiles\f1\OS Firmware\u-boot-usb.imx

 

0 件の賞賛
返信
4 返答(返信)

2,072件の閲覧回数
kishoresamy26
Contributor I

Not using the newer BSP and IMX6G is used

 

 

 

IMX6G 

0 件の賞賛
返信

2,033件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version of bsp are you using? For the board are you using the NXP reference board or the board you designed yourself?

0 件の賞賛
返信

2,075件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Which board and bsp are you using? If you are using the newer BSP, you can use the uuu tool we supply.

0 件の賞賛
返信

2,041件の閲覧回数
kishoresamy26
Contributor I

Not using the newer BSP and IMX6G is used

0 件の賞賛
返信