Why kernel print "alloc_contig_range: [5fc00, 603ea) PFNs busy"?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why kernel print "alloc_contig_range: [5fc00, 603ea) PFNs busy"?

25,918 Views
传策薛
Contributor V

Hi community:

     I am using Android8.1 BSP, when open a app,the debug console print several "alloc_contig_range: [5fc00, 603ea) PFNs busy", at the same time, the app page stuck some time,Is there anyway to fix it ?

14 Replies

16,494 Views
_angelo_
Contributor III

Try 

1) for imx6, check that sdma firmware is really loaded, by dmesg | grep sdma

2) check kernel cma configuration by menuconfig or, try to increase cma arean by "cma=" kernel param

0 Kudos
Reply

16,487 Views
Ratataplam
Contributor II

Hello, seem I have the same problem on imx8mm during WiFi comunication.

After a while the comunication between two board via WiFi goes in blocking but the applications still running  I can connect via serial port with putty.In this case I see :  alloc_contig_range :[....] PFNs busy

The board is not reachable via ping and it's not able to reach any other host also.

I tryed to pull down the WiFi interface and pull-up using the command shell ( ifconfig wlan0 down -> ifconfig wlan0 up) but the comunication is always blocked beside the ifconfig shows UP  state  

The problem is not present if I use the eth interface (cable). Any suggestion?

0 Kudos
Reply

13,041 Views
vincentz63
Contributor IV

Did you ever get to the bottom of this error? We are seeing the exact same thing when using WiFi...

0 Kudos
Reply

17,067 Views
Jahnavi_Guvvala
Contributor I

Hi,

My apologies. I'm new to NXP. what is CMA here? and were you able to resolve this issue?

 

If yes, Please share the fix here. I'm getting the same warning, and my application is crashing when i get this warning.

 

Thanks,

Jahnavi.

0 Kudos
Reply

17,583 Views
tianlj
Contributor I

any news ?

is still not solved?

thanks

0 Kudos
Reply

20,493 Views
m_c
Senior Contributor I

Found similar issue on i.MX6ULLEVK when access ttymxc1.

root@imx6ull14x14evk:~# uname -a
Linux imx6ull14x14evk 4.14.98-imx_4.14.98_2.0.0_ga+g5d6cbea #1 SMP PREEMPT Wed Oct 30 23:55:04 UTC 2019 armv7l GNU/Linux

root@imx6ull14x14evk:~# stty -F /dev/ttymxc1 115200 -parity -cstopb

alloc_contig_range: [90900, 90914) PFNs busy

root@imx6ull14x14evk:~# echo 1234 > /dev/ttymxc1
alloc_contig_range: [90900, 90914) PFNs busy
alloc_contig_range: [90920, 90934) PFNs busy
alloc_contig_range: [90940, 90954) PFNs busy
root@imx6ull14x14evk:~# echo 1234 > /dev/ttymxc1
alloc_contig_range: [90900, 90914) PFNs busy
root@imx6ull14x14evk:~# echo 1234 > /dev/ttymxc1
root@imx6ull14x14evk:~# echo 1234 > /dev/ttymxc1
root@imx6ull14x14evk:~# echo 1234 > /dev/ttymxc1
alloc_contig_range: 8 callbacks suppressed
alloc_contig_range: [90900, 90914) PFNs busy
alloc_contig_range: [90920, 90934) PFNs busy
alloc_contig_range: [90940, 90954) PFNs busy

0 Kudos
Reply

20,493 Views
fabio_poiatti
Contributor III

any news ?

is still not solved?

thanks

0 Kudos
Reply

20,493 Views
Joel69003
Contributor IV

The same here with an other imx6 board, build linux-imx kernel with yocto, warrior branch.

No WiFi on my board, no Ethernet either.

Any body knows the reason of this log ?

Joel

0 Kudos
Reply

20,494 Views
crl6crl6
Contributor III

Still not solved, evk board also has this print.

0 Kudos
Reply

20,494 Views
coindu
Contributor IV

Was the issue solved?

The same issue cause coredump on linux 4.9.88_2.0.0 version

[10219.413664] alloc_contig_range: 85 callbacks suppressed
[10219.413670] alloc_contig_range: [68600, 69601) PFNs busy
[10219.425030] alloc_contig_range: [68600, 69701) PFNs busy
[10219.431136] alloc_contig_range: [68800, 69801) PFNs busy
[10219.437123] alloc_contig_range: [68800, 69901) PFNs busy
[10219.443162] alloc_contig_range: [68800, 69a01) PFNs busy
[10219.449136] alloc_contig_range: [68800, 69b01) PFNs busy
[10219.455168] alloc_contig_range: [68c00, 69c01) PFNs busy
[10219.460887] alloc_contig_range: [68d00, 69d01) PFNs busy
[10219.466670] alloc_contig_range: [68e00, 69e01) PFNs busy
Redistribute latency...
[10219.806379] alloc_contig_range: [72700, 735d5) PFNs busy
[10219.990513] ion-mxc imx_ion: Fail to allocate buffer
Caught SIGSEGV
#0 0x0000ffff9e0f2af4 in poll () from /lib/libc.so.6
#1 0x0000ffff9e1f8a80 in ?? () from /usr/lib/libglib-2.0.so.0
#2 0x000000001e54aac0 in ?? ()
Spinning. Please run 'gdb gst-launch-1.0 11541' to continue debugging, Ctrl-C to quit, or Ctrl-\ to dump core.

0 Kudos
Reply

20,494 Views
传策薛
Contributor V

Still not solved, evk board also has this print

0 Kudos
Reply

20,494 Views
b36401
NXP Employee
NXP Employee

This error may be related to wifi MAC address.
Please try to set MAC address of wifi interface prior to enable it.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

20,494 Views
传策薛
Contributor V

Hi~:

     I dont think so, I found that may be the cma problem when I trace the code?

the evk board also has the problem,you can check it.

20,494 Views
denkraev
Contributor II

Yes, it's about CMA. Got the same message with IMX6 (imx6q-sabresd) Android 8.0 Oreo release.

0 Kudos
Reply