Who must create an android security patch?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Who must create an android security patch?

ソリューションへジャンプ
3,854件の閲覧回数
takayuki_ishii
Contributor V

Hello community,

In  Android Security Bulletins, it have 3 type of security information.

  • Android platform fixes are merged into AOSP 24–48 hours after the security bulletin is released and can be picked up directly from there.
  • Upstream Linux kernel fixes are linked to directly from the bulletin on release and can be picked up from there.
  • Fixes from SOC manufacturers are available directly from the manufacturers.

My understanding that who must apply patches for this 

About "Fixed from SOC manufacturers" will be released some patches from NXP.

Others, "Android platform fixes" and "Upstream Linux kernel fixes", customer must get fixed code for each 

security Bulletins and apply it by themselves.

Is it correct?

Best regards,

Ishii.

ラベル(2)
0 件の賞賛
返信
1 解決策
3,590件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

I think your understanding is correct.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,591件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

I think your understanding is correct.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,590件の閲覧回数
richard_anderse
Contributor I

I have a question about this topic, that might be obvious and is more of an AOSP than a NXP question, but I haven't found a answer to it:

If I have a specific branch i.e. android-9.0.0_r1, does it update itself to r2 if I repo sync? 

As I understand it, every time a new security patch is relased a new release version is made (r1, r2, r3...) and if I want to be up to date with the latest security patch, how do I do?

Best regards,

Richard 

0 件の賞賛
返信
3,590件の閲覧回数
takayuki_ishii
Contributor V

Hello Igor,

Thank you for your answer.

I will answer it to my customer.

Best regards,

Ishii.

0 件の賞賛
返信