Which image has ssh or Telnet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which image has ssh or Telnet

1,315 Views
jeysurier
Contributor I

1. Which of the images (core-image-minimal, core-image-base, fsl-image-gui etc) has ssh or telnet?

2. How can a package management can be added to an image - fsl-image-gui?

Labels (1)
0 Kudos
Reply
1 Reply

1,227 Views
Yuri
NXP Employee
NXP Employee

Hello,

  "fsl-image-gui" and  "fsl-image-qt5" definitely include the SSH and Telnet.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply