Which ECC i.MX6 ROM code uses?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Which ECC i.MX6 ROM code uses?

3,259件の閲覧回数
simonlie
Contributor I

Hello,

I'm using a i.MX6 Solo processor on a custom board. For my bachelor thesis I need to know which ECC the i.MX6 can handle. I want to boot MLO / Barebox from NAND flash. And don't know which ECC I have to provide the MLO / Barebox with. For example, the same problem I had to do for AM335x and there the ROM code uses BCH8.

Maybe somebody know the awnser or can me link a document. In the official Technical Manual i couldn't find any information about it.

Regards,

Simon

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

2,741件の閲覧回数
simonlie
Contributor I

Thank you for the C Code but this is not exactly what I need.

I need to know which ECC the i.MX6 wants to see if it tries to boot from NAND flash. If it is not always the same, where can I get this information from? I think it must be something like Hamming (1-Bit ECC) or BCH(4-40 Bit ECC).

0 件の賞賛
返信

2,741件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please take a look at Chapter 17 [40BIT Correcting ECC Accelerator (BCH)] of the i.MX6 DQ Reference Manual.
The i.MX6 NAND controller (GPMI) uses it.

0 件の賞賛
返信

2,741件の閲覧回数
JerryFan
NXP Employee
NXP Employee

Hi Simon,

i.MX6SL BootROM use different ECC level for FCB(Firmware Config Block) and firmware(such as uboot). For FCB, it is Hamming, and 8 copied of FCB can be supported at most. For firmware, the ECC level can be configured in FCB, the max level is BCH40.

B.R

Jerry

0 件の賞賛
返信