Where is imx6ull ESAI SDK example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is imx6ull ESAI SDK example

1,751 Views
ryan_chen
Contributor II

Hello expert,

Now i'm working on imx6ull platform , i want to implement ESAI  ,but  there are few document  about it , also there is no driver code in "SDK_2.2_MCIM6ULL", 

Can anybody give me some hint ? thanks

0 Kudos
Reply
3 Replies

1,013 Views
cima
Contributor II

I would also appreciate some example. I found various Device tree esai nodes e.g. (e.g. imx6ull.dtsi in linux-imx fork) but it doesn't work for me. It fails with  fsl-esai-dai 2024000.esai: failed to init imx pcm dma: -517 which means to defer the driver loading as it struggles to register DMA channel. There is no documentation and no example to device tree for esai node. 

0 Kudos
Reply

1,724 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @ryan_chen!
Thank you for contacting NXP Support!

All the examples and documentation with that SDK can be downloaded on the next Link:

https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

Chavira_0-1712774549250.png
If that doesn't exist the example you are looking for is unavailable.

Sorry for the mistake!

Best Regards!
Chavira

0 Kudos
Reply

1,709 Views
ryan_chen
Contributor II

Thank you for your prompt response, i overviewed the SDK, there is some examples about sai , but no example refer to esai, what i need is  to enable esai function on bare-metal.

i  have been facting  this problem for many days , it will be very grateful  if you can help me out 

 

@Chavira 

0 Kudos
Reply