Where can I pull all the Android BSP source code for iMX6/Q?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can I pull all the Android BSP source code for iMX6/Q?

2,144 Views
gmmo
Contributor I

I am currently working on an embedded medical device that uses as iMX6Q/D on it main board.

The chip runs Android OS Linux version 3.0.35 (JellyBean ), more precisely we are using this google kernel:

android-4.3_r2.1

JSS15J android-4.3_r2.1 Jelly Bean Nexus 7 (flo/deb)

The imx_kernel part comes from all thee way back when NXP was Freescale and it is still avaiable using this repo:

git clone git://git.freescale.com/imx/linux-2.6-imx.git kernel_imx
and the tag is jb4.3_1.1.0-ga

We are stuck in some "Surfaceflinger" coming from "hwcomposer_viv.imx6.so" crash. Can anyone can point me in how to pull latest hwcomposer_viv for our current BSP

Long story short can someone show me how to pull the NXP code of the hwcomposer_viv and all its branches?

I see these links but when I unzip is it just a bunch of "git diffs". Where is the source?

https://www.nxp.com/products/processors-and-microcontrollers/applications-processors/i.mx-applicatio...


Is there any documentation showing where to pull all the Android BSP source code and it branches. Again the only thing I see are "git diffs" :smileysad: 

thank you.

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

1,583 Views
jimmychan
NXP TechSupport
NXP TechSupport
0 Kudos
Reply