Where can I find the file FEC_BlockGuide.pdf?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where can I find the file FEC_BlockGuide.pdf?

1,640件の閲覧回数
FredrikMoller
Contributor III

The reference manual for the Ethernet controller on i.MX28 says in chapter 26.2.2:

This section provides the technical details for the uDMA. Additional details required for

legacy mode compatibility is provided in the FEC specification (FEC_BlockGuide.pdf).

Where can I find this FEC specification?

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,446件の閲覧回数
Yuri
NXP Employee
NXP Employee

You may use FEC chapters of i.MX25 and i.MX27 Reference Manual - they are based on the same FEC_BlockGuide.pdf.

http://cache.freescale.com/files/dsp/doc/ref_manual/IMX25RM.pdf?fpsp=1

http://cache.freescale.com/files/32bit/doc/ref_manual/MCIMX27RM.pdf?fpsp=1