I have a need to run Android on a Linux 3.10 (or later) kernel for hardware support reasons. I know the Android 4.4.3 in Freescale's repositories is using 3.10.? kernel. I have the kernel and u-boot code from branch kk4.4.3_2.0.0-ga. I'm still using the beta android patches from Freescale. Unfortunately, it won't load Android.
Does anyone know when (beyond just Feb-2015) the Android general availability release will be available? This is becoming critical for us.
Thanks,
Greg
解決済! 解決策の投稿を見る。
Hello Gregory,
It is scheduled for February 6th by end of day.
Where can I obtain the code and patches?
ooops, sorry. I found it.
You can download it from here:
i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale
Under: "Run time software" >> "operating system software" >> IMX6_KK443_200_ANDROID_SOURCE_BSP
Have a great day,
Sergio
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi SergioSolis
I have downloaded the KK4.4.3 BSP.
but where I can fetch the documents for reference, something like IMX6_KK442_100_ANDROID_DOCS from i.MX 6 D/Q/DL/S/SL kk4.4.2_1.0.0 GA release
Thanks
Bateman
Hi
Sergio
What will be the kernel version used?
I'm sorry for the late response, it is 3.10.53.
Have a great day,
Sergio
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------