When u-boot to kernel driver LVDS will flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When u-boot to kernel driver LVDS will flash

2,428 Views
wangtsungli
Contributor IV

Hi community,

I'm working on i.MX6 Quad sabre-SD platform and build Android 6 as my image.

Here is the situation I need help.

I enable LVDS in u-boot and show LOGO.

But when system turn u-boot form kernel driver, panel will flash and change to another LOGO.

Changing to another LOGO is okay but I do not want panel be flashed once.

How can I avoid flash issue?

Thanks in Advanced!

0 Kudos
Reply
3 Replies

2,185 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Is this i.MX6 Quad sabre-SD patform you designed yourself or buy from NXP?

0 Kudos
Reply

2,185 Views
wangtsungli
Contributor IV

I buy one platform from NXP and designed one for myself.

The problem occurred on my designed platform.

But the same issue occurred on platform which I bought from NXP.

0 Kudos
Reply

2,185 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

OK, I will test it on our reference board and do further confirm it for you.

0 Kudos
Reply