When might the VPU H.264 Encoder use FMO/ASO/RS Baseline Profile Features?
I'm producing a video stream targeted for digital TVs, some of which do not support H.264 Baseline Profile features FMO (flexible macroblock ordering), ASO (arbitrary slice ordering) and RS (redundant slices).
When might the VPU H.264 Encoder use these features, and is it possible to eliminate this use? I'm currently using the Yocto Dylan release with the corresponding meta-fsl-arm branch. I'm controlling the VPU via the VPUENC gstreamer plugin.
Hello,
Unfortunately we do not have a date to share with you at this moment. I apologize for the inconvenience.
Have a great day,
Jaime
-------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-------------------------------------------------------------------------------