[Background]
The LCD resolution is 1280x720, so we need capture Camera video as 1280x720 via V4L2 interface.When we capture the camera, find the warning messages "imx-ipuv3 imx-ipuv3.0: IDMAC9's EBA0 is not 8-byte aligned" scroll on serial console frequently, the camera screen is splitted in the vertical middle of screen, detailed see attached files.
BTW,another LCD resolution is 800x480, there is no warning message and the camera screen is normal.
[Question]
How to show the normal camera screen via V4L2 on LCD resolutin of 1280x720
[Related code]
If ((fd_output_v4l = open("video17", O_RDWR, 0)) < 0)
{
ERROR("Unable to open %s\n", EARLY_RVC_DEV_VD_OUPTPUT);
return -1;
}
crop.type = V4L2_BUF_TYPE_VIDEO_OUTPUT;
crop.c.top = top;
crop.c.left = left;
crop.c.width = width;
crop.c.height = height;
if (ioctl(fd_output_v4l, VIDIOC_S_CROP, &crop) < 0)
{
ERROR("set crop failed\n");
return -1;
}
Hi Youfu
please recheck that lcd is correctly integrated using examples below
https://community.freescale.com/thread/355690
https://community.freescale.com/thread/373763
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you igor for your reply my question
We use kernel version on 3.0.35.
Our LCD Panel via LDB interface show the correct 1280x720 resolution when not show camera.
The warning message “imx-ipuv3 imx-ipuv3.0: IDMAC9's EBA0 is not 8-byte aligned” only show when capture camera on v4l2 overlay.
It may be concerned with the non-aligned accesses
Best regards
youhu hu
I believe one can try to check sources csi_v4l2_overlay.c
Index of /buildsources/i/imx-test/imx-test-3.0.35-4.0.0
Best regards
igor
Thanks igor for your suggestion。
Our product don't use overlay mode, but use output mode,Some as Index of /buildsources/i/imx-test/imx-test-3.0.35-4.0.0 imx-test-3.0.35-4.0.0\test\mxc_v4l2_testmxc_v4l2_output.c
We compile this mxc_v4l2_testmxc_v4l2_output.c soucecode with gcc, but it failed when
1-1. cropcap.type = V4L2_BUF_TYPE_VIDEO_OUTPUT;
if (ioctl(fd_v4l, VIDIOC_CROPCAP, &cropcap) < 0)
{
printf("get crop capability failed\n");
retval = TFAIL;
goto err1;
}
We checked our kernel 3.0.35 mxc_v4l2_capture.c, the cropcap.type = V4L2_BUF_TYPE_VIDEO_OUTPUT is not supported
,So delete it
case VIDIOC_CROPCAP: {
struct v4l2_cropcap *cap = arg;
pr_debug(" case VIDIOC_CROPCAP\n");
if (cap->type != V4L2_BUF_TYPE_VIDEO_CAPTURE &&
cap->type != V4L2_BUF_TYPE_VIDEO_OVERLAY) {
retval = -EINVAL;
break;
}
cap->bounds = cam->crop_bounds;
cap->defrect = cam->crop_defrect;
break;
}
1-2. Also we have deleted this code because our yuv raw file dont have header.
if (g_bmp_header) {
fseek(in, 0x36, SEEK_CUR);
}
1-3. Change the default fmt to UYVY
uint32_t g_in_fmt = V4L2_PIX_FMT_UYVY;
Detailed see the mxc_v4l2_output.c which I will post.
2.Execute command
./mxc_v4l2_output -d /dev/video17 -iw 720 -ih 480 -ow 1280 -oh 720 -ot 0 -ol 0 -l 10000 /udisk1/f3.yuv
find the warning messages "imx-ipuv3 imx-ipuv3.0: IDMAC12's EBA0 is not 8-byte aligned" scroll on serial console frequently, the yuv content screen is splitted in the vertical middle of screen, detailed see attached files show_result1.jpg、show_result2.jpg 。
So How to fix it