What onboard USB controller is implemented into i.MX 8m?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What onboard USB controller is implemented into i.MX 8m?

957件の閲覧回数
contact3
Contributor I

What implementation you are using internally as the USB host controller on the i.MX 8M series? EX, Intel/ASmedia... version number, etc. This is not mentioned on your data sheets. Thank you very much! 

ラベル(1)
タグ(4)
0 件の賞賛
返信
3 返答(返信)

780件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ty

seems this is designware cores, as one can find its

references in sect.11.1.3.23.2 Diagram  - "DWC_*"    i.MX8MDQ Reference Manual
https://www.nxp.com/webapp/Download?colCode=IMX8MDQLQRM&Parent_nodeId=1480454149826718646460&Parent_... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

780件の閲覧回数
contact3
Contributor I

Thank you muchly igor, though the link currently does not work.

0 件の賞賛
返信

780件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信