What onboard USB controller is implemented into i.MX 8m?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What onboard USB controller is implemented into i.MX 8m?

1,404 Views
contact3
Contributor I

What implementation you are using internally as the USB host controller on the i.MX 8M series? EX, Intel/ASmedia... version number, etc. This is not mentioned on your data sheets. Thank you very much! 

Labels (1)
0 Kudos
Reply
3 Replies

1,227 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ty

seems this is designware cores, as one can find its

references in sect.11.1.3.23.2 Diagram  - "DWC_*"    i.MX8MDQ Reference Manual
https://www.nxp.com/webapp/Download?colCode=IMX8MDQLQRM&Parent_nodeId=1480454149826718646460&Parent_... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,227 Views
contact3
Contributor I

Thank you muchly igor, though the link currently does not work.

0 Kudos
Reply

1,227 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply