Hi community,
Our partner have a question about i.MX6DL G2D API.
When use i.MX6DL G2D API, can we set the scaling ratio liberally?
Or is there some restriction?
(e.g. The scaling ration have to be a multiple or submultiple number of 2 (x2, x4, x1/2, 1/8, etc...))
Best Regards,
Satoshi Shimoda
Hi Satoshi,
yes one can choose any scaling ratio, no restricitons.
Document i.MX_6_2D_API.pdf (included in Doc bundle on link below)
in sect.8.6 "Filter BLT" states:
"Filter blit performs high quality scaling, up or down, using an FIR re-sampling
filter with up to 9 taps. Sub-pixel coordinates (locations between the pixel grids)
are generated by the drawing engine.
..
A stretch- or shrink-factor of 15.16 fixed-point format is supported."
L3.10.17_1.0.0_LINUX_DOCS
Linux 3.10.17 BSP & MM Bundle
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------