linux version : 3.0.35
./ltib/rpm/BUILD/linux/arch/arm/mach-mx6/mx6_ddr_freq.S (line 485)
/* if DLL is currently on, turn it off
cmp r9, #1
beq continue_dll_off_1
There is an commented block but comment is not closed, is it right?
The commented code does not make trouble but looks untrustworthy,
Best regards.
Solved! Go to Solution.
Hi JHY
this (unfinished comment) was fixed in latest L3.0.101_4.1.1 release:
ENGR00320182 [iMX6DQ/iMX6DL] Fix bug in DLL off mode code in DDR3 frequency change procedure
L3.0.101_4.1.1_SOURCE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Linux BSP Source Code Files.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi JHY
this (unfinished comment) was fixed in latest L3.0.101_4.1.1 release:
ENGR00320182 [iMX6DQ/iMX6DL] Fix bug in DLL off mode code in DDR3 frequency change procedure
L3.0.101_4.1.1_SOURCE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Linux BSP Source Code Files.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------