Weight Information required ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Weight Information required ?

1,234 Views
mp_manickarajan
Contributor I

Weight Information required for 8909009731

MX8DualX4 Processor - CPU, FCPBGA, 21 × 21 mm, 0.8 mm pitch

Thanks,

Manick

0 Kudos
Reply
1 Reply

1,147 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Manick,

The weight is obtained from the sum of masses indicated on the Material Declaration document of each part number. Taking as example, the MCIMX6QP6AVT1AB (i.MX6QuadPlus whit the same 0.8mm pitch; 21mm x 21mm package) is available on the link below:

https://www.nxp.com/mcds/MCIMX6QP6AVT1AB.pdf

For the specific case of the part number that you are looking for, it will be required contacting with your Sales/FAE, because i.MX8X is still on preproduction and no additional information/support could be provided yet though this channel.


Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 Kudos
Reply