Wayland image on i.MX8QXP MEK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Wayland image on i.MX8QXP MEK

2,728 次查看
ajmalali
Contributor III

Hi,

I am trying to build Qt 5 Weston Wayland image for i.MX8QXP. I have followed the document "i.MX Yocto Project User's Guide, rev : L4.9.51_8qm-beta2/8qxp-beta, 02/2018". The steps i followed is listed below,

$ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-morty -m imx-4.9.51-8qm_beta2.xml

$ repo sync

$ DISTRO=fsl-imx-wayland MACHINE=imx8qxpmek source fsl-setup-release.sh

$ bitbake fsl-image-qt5-validation-imx

As suggested in the document.

The Yocto build was completed successfully. However the rootfs generated does not have weston in it. I flashed the generated binaries in the SD card and was able to boot successfully, but there was no display. What am i doing wrong. Do i need to add anything in the "local.conf" of the build.

Regards,

Ajmal

0 项奖励
回复
2 回复数

2,346 次查看
ajmalali
Contributor III

Hi,

I was able to build Qt 5 Weston Wayland image for i.MX8QXP with the 4.9.88 release. The repo was init from a different branch.

Regards,

Ajmal

0 项奖励
回复

2,346 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Unfortunately the i.MX8QXP it is under PRE-PRODUCTION, this means that the silicon revision it is not final, and we are still having changes either Software and Hardware for the release of the device.  Please contact your local NXP Distributor or your local NXP Sales Representative so they can provide support for this device at the moment.

I apologize for any inconvenience.

0 项奖励
回复